Skip to main content
Graduate
November 20, 2023
Solved

I have a question about the CAN filter numbering diagram in the RM0316 Reference manual

  • November 20, 2023
  • 2 replies
  • 1194 views

Hi 

 

In the figure below, FIFO1 filter bank 7 and filter bank 10 have the same settings. If the ID list is 16bit, I think it is correct to have 4 Filter Nums. There are two filter banks 7, 4 and 5. Is this correct?

 

can.PNG

    This topic has been closed for replies.
    Best answer by KDJEM.1

    Hello @Ukazu ,

    Thank you fringing this issue to our attention.

    Figure 394. in RM0316 is wrong and should be:

    KDJEM1_0-1700663000882.png

    Filter bank 7 and filter bank 10 haven't the same settings.

    Filter bank 7: Deactivated ID Mask (16-bit), Filter Num 4, 5

    Filter bank 10: Deactivated ID List (16-bit), Filter Num 8,9,10,11.

    I reported this typo internally.

    Internal ticket number: 166948 (This is an internal tracking number and is not accessible or usable by customers).

    Thank you.

    Kaouthar

     

     

    2 replies

    Technical Moderator
    November 20, 2023

    Hi @Ukazu ,

    Thank you for posting this issue.

    I will check internally and I will get back to you with more details as soon as possible.

    Thank you.

    Kaouthar

    KDJEM.1Answer
    Technical Moderator
    November 22, 2023

    Hello @Ukazu ,

    Thank you fringing this issue to our attention.

    Figure 394. in RM0316 is wrong and should be:

    KDJEM1_0-1700663000882.png

    Filter bank 7 and filter bank 10 haven't the same settings.

    Filter bank 7: Deactivated ID Mask (16-bit), Filter Num 4, 5

    Filter bank 10: Deactivated ID List (16-bit), Filter Num 8,9,10,11.

    I reported this typo internally.

    Internal ticket number: 166948 (This is an internal tracking number and is not accessible or usable by customers).

    Thank you.

    Kaouthar

     

     

    UkazuAuthor
    Graduate
    November 26, 2023

    @KDJEM.1 

    Thank you.

    This modification is as per the documentation.
    I have no doubts.

     

    This thread will be closed.