i want to get the message from the uart every 5s. how can i configure timer based on that
clock frequency 170MHz
This is the code i have generated using TIM2 CH1
could you please set the prescalar, period,pulse to get output every 5s
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 169;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 9999;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 9999;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
//motor1State = MC_GetSTMStateMotor1();
HAL_TIM_Base_Start(&htim2);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
//motor1Faults = MC_GetOccurredFaultsMotor1();
motor1Faults = MC_GetCurrentFaultsMotor1();
switch (motor1Faults)
{
case 0:
HAL_UART_Transmit_DMA(&huart2, "MC_NO_ERROR", 12);
break;
case 1:
HAL_UART_Transmit_DMA(&huart2, "MC_DURATION", 12);
break;
case 2:
HAL_UART_Transmit_DMA(&huart2, "MC_OVER_VOLT", 13);
break;
case 4:
HAL_UART_Transmit_DMA(&huart2, "MC_UNDER_VOLT", 14);
break;
case 8:
HAL_UART_Transmit_DMA(&huart2, "MC_OVER_TEMP", 13);
break;
case 10:
HAL_UART_Transmit_DMA(&huart2, "MC_START_UP", 12);
break;
case 20:
HAL_UART_Transmit_DMA(&huart2, "MC_SPEED_FDBK", 14);
break;
case 40:
HAL_UART_Transmit_DMA(&huart2, "MC_BREAK_IN", 12);
break;
case 80:
HAL_UART_Transmit_DMA(&huart2, "MC_SW_ERRORS",12);
break;
}
/* USER CODE END TIM2_Init 2 */
HAL_TIM_MspPostInit(&htim2);
}