I2C issue when called from external file
Hi There,
We have IO expander that is connected using I2C
File: Application.C has functions for change the IO value of the IO Expander
there is a UART that the user can connect to and change the value of the IO Expander (using CLI)
Following functions are at Application.C file
void PORT_Enable(uint8_t PORT_NUM){
switch (PORT_NUM){
case PORT1:
Set_Bit_IO_Expander2_Status_PDIO(PDIO_Status,PORT_NUM);
PORT_Information[PORT_NUM].Enable_VBUS = 1;
break;
}
}
void Set_Bit_IO_Expander2_Status_PDIO(uint8_t Data,uint8_t Index)
{
PDIO_SET_RESET[0] = OUTPUT_PORT1; //write command to output Port 1.0-1.7
Data |= (1 << Index); // implement '1' into bit#index
PDIO_SET_RESET[1] = Data; //update byte to send to Set Port 1.0-1.7
while (HAL_I2C_GetState(&hi2c2) != HAL_I2C_STATE_READY){}
pcal9555_writeRegister(&hi2c2, 0x42, PDIO_SET_RESET, 2);
}
the following function are at COM.C file
void executeSerialCommand1(char *uart1RxBuf)
{
if(strcmp(uart1RxBuf,"port3 Enable") == 0){
PORT_Enable(3);
}
there is a loop with timmer that read the IO Expander's pins every 100mSec
this code is at Application.C file
void Application_Handler(void)
{
////////////////////////////////////////////////////////////////////////////
//Do every 10ms
////////////////////////////////////////////////////////////////////////////
if (TimeElapsed_10ms)
{
TimeElapsed_10ms = 0;
}
////////////////////////////////////////////////////////////////////////////
//Do every 100ms
////////////////////////////////////////////////////////////////////////////
if (TimeElapsed_100ms)
{
TimeElapsed_100ms = 0;
Update_Port_Params();
}
}
on startup, the system set all ports to '1'
therefore, there is no issue with "PORT_Enable()" function when calling it from the Application.C file
when using the UART to set port3 the application doesn't work properly and enters a loop
We use IO_Expander.C file for activating I2C communication
HAL_StatusTypeDef pcal9555_writeRegister(I2C_HandleTypeDef *hi2c, uint16_t address, uint8_t *pData, uint16_t Size){
// HAL_Status = HAL_I2C_Master_Transmit_IT(hi2c,(uint16_t) ADT7411_ADDRESS, pData, Size);
//return HAL_Status;
HAL_Status = HAL_I2C_Master_Transmit_IT(hi2c,address, pData, Size);
while (HAL_I2C_GetState(hi2c) != HAL_I2C_STATE_READY){
/* Error_Handler() function is called when Timeout error occurs.
When Acknowledge failure occurs (Slave don't acknowledge its address)
Master restarts communication */
if ((HAL_I2C_GetError(hi2c) != HAL_I2C_ERROR_AF) && (HAL_I2C_GetError(hi2c) != HAL_I2C_ERROR_NONE))
{
Error_Handler();
}
}
return HAL_Status;
}
it seams that HAL_Status is not READY when calling it from the UART so it has a loop at
while (HAL_I2C_GetState(hi2c) != HAL_I2C_STATE_READY){
when we call the function from the Application.C file, there is no issue
print of the Watch list at the While statment:

any advice will be appreciated
thank you