Skip to main content
Explorer
February 14, 2025
Solved

I2C Slave device implementation ACK/NACK problem

  • February 14, 2025
  • 3 replies
  • 1106 views

As mentioned in the topic subject, I would like to implement I2C Slave device which will simulate the BQ769x2 device. For development I'm using STM32F4 Discovery board, but the final product will be deployed on STM32L0.

Master device is first trying to detect if slave device is present and after that some functions will be called in no exact order nor the functions have same length. Therefore I was thinking interrupt mode would be appropriate to implement here for greater control.

For testing purpose I have written small Master device program for Arduino (running on Arduino MKRZERO).
With this example one can send scan or probe command over serial to run the procedure.

 

 

#include <Wire.h>
#include <stdarg.h>
#define PRINTF_BUF 80 // define the tmp buffer size (change if desired)

String inputData;

void setup() {
 Wire.begin();
 Wire.setClock(100000);
 #if defined(WIRE_HAS_TIMEOUT)
 Wire.setWireTimeout(300 * 1000 /* us */, true /* reset_on_timeout */);
 #else
 Wire.setTimeout(500);
 #endif

 Serial.begin(115200);
 while(!Serial)
 delay(10);
 Serial.println("\nI2CScanner started");
}

void loop() {
 // wait for user input
 while(Serial.available() == 0){}

 inputData = Serial.readString();
 inputData.trim();

 if(inputData.equals("scan"))
 {
 Serial.println(inputData);
 i2cdetect();
 }
 else if(inputData.startsWith("probe"))
 {
 uint8_t err = probe(0x48);
 if(!err)
 {
 Serial.println("No error...");
 }
 else
 {
 Serial.print("\nError probing with error: ");
 Serial.println(err);
 }
 }
}

uint8_t probe(uint8_t address)
{
 Wire.beginTransmission(address);
 Wire.write(0x3E);
 Wire.write(0x01);
 Wire.write(0x00);
 uint8_t err = Wire.endTransmission(1);
 return err;
}

void i2cdetect()
{
 uint8_t first = 1, 
 last = 127;
 uint8_t i, j, address, error;

 // header
 Serial.print(" ");
 for (i = 0; i < 16; i++) {
 printf("%3x", i);
 }
 Serial.println("");

 // body
 for (j = 0; j < 8; j++) {
 _printf("%02d:", j*10);
 for (i = 0; i < 16; i++) {
 address = i + j*16;
 if (address >= first && address <= last) {
 Wire.beginTransmission(address);
 error = Wire.endTransmission();
 if (error) {
 Serial.print(" --");
 } else {
 _printf(" %02x", address);
 }
 } 
 else {
 Serial.print(" ");
 }
 }
 Serial.println("");
 }
}

void _printf(const char *format, ...)
{
 char buf[PRINTF_BUF];
 va_list ap;
 va_start(ap, format);
 vsnprintf(buf, sizeof(buf), format, ap);
 for(char *p = &buf[0]; *p; p++) // emulate cooked mode for newlines
 {
 if(*p == '\n')
 Serial.write('\r');
 Serial.write(*p);
 }
 va_end(ap);
}

 

 


This is (with different address) what Master should create:

mr4k_0-1739542590631.png

As you can see, here the example shows clock stretching - I have to work without this functionality.

The problem is, that my STM32 program is not working properly. The code for I2C slave device is provided below.
If HAL_Delay is called, the ACK is sent, but HAL_I2C_ListenCpltCallback is not called. If delay is not present the NACK is generated and Master can not proceed as desired.

Write_3E_0100_NACK1.png

This is what I can see on my oscilloscope after probe procedure is called on the master in case of no delay in the STM32 code and bellow in case when delay is present in STM32 code.

Write_3E_0100_ACK.png
But as said, if ACK is sent STM does not call HAL_I2C_ListenCpltCallback (as it should?) and in case of NACK master can't go on (in real life situation).

Here are parts of my STM32F4 code:

 

/*
 * STM32_I2C_Slave.c
 */

/* include */
#include "I2C_Slave.h"
#include "registers.h"
#include "protocol.h"
#include "stdio.h"
#include "string.h"

volatile i2c_t I2C_slave_obj;

uint8_t buff[2] = {0x00, 0x00};

uint32_t maxBusyDelay = 150;
uint32_t maxCMDDelay = 500; // delay in MS

uint32_t lastAddrCallback = 0;
uint8_t readRegAddress = 1;
uint8_t allowTX = 0;
uint8_t indexRA = 0;

void i2c_slave_clear(void){
	I2C_slave_obj.reg_address = 0;
	I2C_slave_obj.reg_addr_rcvd = 0;
	I2C_slave_obj.payload = 0;
	I2C_slave_obj.curr_idx = NONE;
}

void i2c_slave_init(I2C_HandleTypeDef *hi2c)
{
	I2C_slave_obj.i2c_handler = hi2c;
	i2c_slave_clear();
	HAL_I2C_EnableListen_IT(hi2c);
}

void i2c_slave_check_timeout(void)
{
	static int rx_busy_counter = 0;
	HAL_I2C_StateTypeDef status = HAL_OK;

	status = HAL_I2C_GetState(I2C_slave_obj.i2c_handler);
 if (status == HAL_I2C_STATE_BUSY_RX_LISTEN) rx_busy_counter++;
 else rx_busy_counter = 0;
 if (rx_busy_counter > 150)
 {
 HAL_I2C_DisableListen_IT(I2C_slave_obj.i2c_handler);
 HAL_I2C_DeInit(I2C_slave_obj.i2c_handler);
 HAL_I2C_Init(I2C_slave_obj.i2c_handler);
 HAL_I2C_EnableListen_IT(I2C_slave_obj.i2c_handler);
 rx_busy_counter = 0;
 }

 if(lastAddrCallback + maxCMDDelay > HAL_GetTick())
 {
 readRegAddress = 0;
 lastAddrCallback = 0;
 HAL_GPIO_WritePin(LD5_GPIO_Port, LD5_Pin, GPIO_PIN_RESET);
 }
 else
 {
 readRegAddress = 1;
 }
}

void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode){
 if(AddrMatchCode == I2C_slave_obj.i2c_handler->Init.OwnAddress1)
 lastAddrCallback = HAL_GetTick();

 if(TransferDirection == I2C_DIRECTION_TRANSMIT)
 {
 // MASTER / Controller wants to write
 // can write CMD or just I2CDetect probing
 if(readRegAddress)
 {
 //HAL_I2C_Slave_Receive_IT(hi2c, (uint8_t*)&I2C_slave_obj.reg_addr_rcvd, 3);
 if(HAL_I2C_Slave_Seq_Receive_IT(hi2c, (uint8_t*)&I2C_slave_obj.reg_addr_rcvd, 1, I2C_FIRST_FRAME) != HAL_OK)
 {
 HAL_I2C_ErrorCallback(hi2c);
 }
 else
 {
 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
 }
 }
 }
 else
 {
 // MASTER / Controller wants to read
 // we will need to send appropriate data to MASTER / Controller
 HAL_I2C_Slave_Seq_Receive_IT(hi2c, buff, 2, I2C_LAST_FRAME);
 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
 }

	HAL_I2C_EnableListen_IT(hi2c);
}

void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *hi2c){

 if(!I2C_slave_obj.reg_addr_rcvd)
 {
 // If reg_addr_rcvd = 0 its probably I2CDetect probing
 readRegAddress = 1;
 }
 else
 {
 switch(I2C_slave_obj.reg_addr_rcvd)
 {
 case 0x3E:
 //HAL_I2C_Slave_Receive_IT(hi2c, &buff[0], 2);
 if(HAL_I2C_Slave_Seq_Receive_IT(hi2c, &buff[indexRA], 1, (!indexRA) ? I2C_NEXT_FRAME : I2C_LAST_FRAME) != HAL_OK)
 {
 HAL_I2C_ErrorCallback(hi2c);
 }
 else
 {
 indexRA++;
 if(indexRA==2)
 {
 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
 }
 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
 // HAL_Delay(20); 
 // this delay allows to make ACK ?... but ListenCpltCallback still not called
 }
 break;
 default:
 readRegAddress = 1;
 indexRA = 0;
 lastAddrCallback = 0;
 }
 }

 if(indexRA == 2)
 {
 readRegAddress = 1;
 indexRA = 0;
 lastAddrCallback = 0;
 }

	HAL_I2C_EnableListen_IT(hi2c);
}

void HAL_I2C_AbortCpltCallback (I2C_HandleTypeDef *hi2c){
	HAL_I2C_EnableListen_IT(hi2c);
}

void HAL_I2C_ListenCpltCallback (I2C_HandleTypeDef *hi2c)
{
 HAL_GPIO_TogglePin(LD6_GPIO_Port, LD6_Pin);
 HAL_GPIO_WritePin(LD3_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);
 HAL_I2C_EnableListen_IT(hi2c);
}

void HAL_I2C_SlaveTxCpltCallback(I2C_HandleTypeDef *hi2c){
	I2C_slave_obj.reg_addr_rcvd = 0;
	I2C_slave_obj.reg_address = 0;

	HAL_I2C_EnableListen_IT(hi2c);
}

void HAL_I2C_ErrorCallback(I2C_HandleTypeDef *hi2c)
{
 HAL_GPIO_WritePin(LD5_GPIO_Port, LD5_Pin, GPIO_PIN_SET);

	uint32_t error_code = HAL_I2C_GetError(hi2c);
	uint32_t BERR = (error_code & HAL_I2C_ERROR_BERR);
	uint32_t ARLO = (error_code & HAL_I2C_ERROR_ARLO);
	uint32_t AF = (error_code & HAL_I2C_ERROR_AF);
	uint32_t OVR = (error_code & HAL_I2C_ERROR_OVR);
	uint32_t DMAE = (error_code & HAL_I2C_ERROR_DMA);
	uint32_t TOUT = (error_code & HAL_I2C_ERROR_TIMEOUT);
	uint32_t SIZE = (error_code & HAL_I2C_ERROR_SIZE);
	uint32_t DMA = (error_code & HAL_I2C_ERROR_DMA_PARAM);
	uint32_t STR = (error_code & HAL_I2C_WRONG_START);

	if (BERR)
	{
	 HAL_GPIO_TogglePin(LD5_GPIO_Port, LD5_Pin);
	 HAL_I2C_DisableListen_IT(hi2c);
 HAL_I2C_DeInit(hi2c);
 HAL_I2C_Init(hi2c);
 HAL_I2C_EnableListen_IT(hi2c);
	}
	else if (AF)
	{
	 // I2CDetect was called most probably
		__HAL_I2C_CLEAR_FLAG(hi2c, I2C_FLAG_AF);
		readRegAddress = 1;
		lastAddrCallback = 0;
		I2C_slave_obj.reg_addr_rcvd = 0;
		memset(buff, 0, sizeof(buff));
	}
	HAL_I2C_EnableListen_IT(hi2c);
}

/////// this is from main.c
int main(void)
{
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_I2S3_Init();
 MX_USB_HOST_Init();
 MX_I2C1_Init();

 //Init i2c-slave and call HAL_I2C_EnableListen_IT inside
 i2c_slave_init(&hi2c1);

 while (1)
 {
 // check for timeouts
 i2c_slave_check_timeout();
 // all other code for I2C is handled in I2C_Slave

 MX_USB_HOST_Process();
 }
}

// and init functions for clk and i2c
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

static void MX_I2C1_Init(void)
{
 hi2c1.Instance = I2C1;
 hi2c1.Init.ClockSpeed = 100000;
 hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c1.Init.OwnAddress1 = 144;
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 Error_Handler();
 }
}

 


Looks like I'm handling something wrong or some flags are not cleared as they should be... maybe __disable_irq/__enable_irq at some point... using interrupts only for setting flags and implement logic in main program... I don't know anymore :)
Also I'm not sure if HAL_I2C_EnableListen_IT should be really called in all those places.

I hope I was clear with my question - head is allover the place right now.

Basically - I would like to support i2cdetect (in a way that STM32 will not stuck) and presented command in first picture. Right now - or slave or master don't work as desired. 

Thanks for help in advance.

    This topic has been closed for replies.
    Best answer by mr4k

    Answering to myself and potential readers again.
    What have solved my transmitting from slave to master issue was the pull-up resistor (8kOhm).
    Pull-up resistor can be further optimized based on real application I believe.
    Nevertheless, now in test environment I can communicate in both directions with enabled or disabled clock stretching.

    So to avoid problems (note to readers and myself):

    • call HAL_I2C_EnableListen_IT at start and after every HAL_I2C_ListenCpltCallback (or HAL_I2C_AbortCpltCallback).
    • make sure you have sufficient pull-up on both SDA and SCL lines (more details in manuals) to ensure stable communication.
    • handle state machine logic (if any) in main loop and exit from interrupt routine as soon as possible.

    This topic can be closed now.

    3 replies

    Super User
    February 14, 2025

    Start from an example that works and use that code as a template.

    STM32CubeF4/Projects/STM32F4-Discovery/Examples/I2C/I2C_TwoBoards_RestartAdvComIT/Src/main.c at 57d6d1cd0488d2572982edffc2e23b1df471374b · STMicroelectronics/STM32CubeF4

     

    > HAL_I2C_DeInit(hi2c);
    > HAL_I2C_Init(hi2c);

    It is not good to have stuff like this in your code. If anything, it will silently hide the error happening. Solve the error instead.

    mr4kAuthor
    Explorer
    February 15, 2025

    Thanks for your reply @TDK .
    I'm aware of this example, now I have taken it as base code and make changes according to my example.
    What I have notice I was doing wrong is calling HAL_I2C_EnableListen_IT in places I should not.
    I have also make sure that the output speed for GPIO port is set to very fast and give it the priority of 0 (as in the linked example).
    Now the the command from master can be received. 
    Next, when CLK stretching is disabled (on STM32 as slave9, I got OVR FLAG when calling seq_transive_it function and can not recover from it as flag can not be cleared. But this is somehow expected according to errata. Therefore I tried to enable the CLK stretching and after that the transfer seems to start but nothing is really happening (it stucks here). I believe that this is somehow HW/wiring error? Will have to check what is going on, but I'm without instruments at the moment.

    In real life situation I will not have the availability to have CLK stretching enabled. What are my options then? 

    This limitation can occur only under the following conditions:
    • in Target transmit mode
    • with clock stretching disabled (NOSTRETCH = 1)
    • if the software is late to write to the DR data register, but not late enough to set the OVR flag (the data
    register is written before)
    
    If the controller device does not allow it, ensure that the software is fast enough when polling the TXE or ADDR
    flag to immediately write to the DR data register. For instance, use an interrupt on the TXE or ADDR flag and
    boost its priority to the higher level.

    I don't fully understand what are my options, as I set the priority of the interrupt at 0 (highest), and data for transition is available when AddrCallback is registered. Or should I call hi2c->Instance->DR before HAL_I2C_Slave_Seq_Transmit_IT?

    Thanks 

    mr4kAuthorAnswer
    Explorer
    February 17, 2025

    Answering to myself and potential readers again.
    What have solved my transmitting from slave to master issue was the pull-up resistor (8kOhm).
    Pull-up resistor can be further optimized based on real application I believe.
    Nevertheless, now in test environment I can communicate in both directions with enabled or disabled clock stretching.

    So to avoid problems (note to readers and myself):

    • call HAL_I2C_EnableListen_IT at start and after every HAL_I2C_ListenCpltCallback (or HAL_I2C_AbortCpltCallback).
    • make sure you have sufficient pull-up on both SDA and SCL lines (more details in manuals) to ensure stable communication.
    • handle state machine logic (if any) in main loop and exit from interrupt routine as soon as possible.

    This topic can be closed now.