Skip to main content
Graduate
July 22, 2024
Solved

I3C Dynamic Address

  • July 22, 2024
  • 1 reply
  • 1049 views

I'm using the I3C_Controller_ENTDAA_IT example to assign dynamic addresses to two BMA530 sensors, but I'm getting errors when running the code. Are there any modifications or additional steps I should consider to resolve this issue? I haven't made any modifications or additions yet.

Azad_0-1721655184264.png

 

    This topic has been closed for replies.
    Best answer by Azad

    Sorry, my mistake. I needed to load both the controller_entdaa_it and target_entdaa_it codes for the ENTDAA command to work. I had only loaded controller_entdaa_it. The problem is solved now.

    1 reply

    ST Employee
    July 24, 2024

    This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly

    AzadAuthorAnswer
    Graduate
    July 30, 2024

    Sorry, my mistake. I needed to load both the controller_entdaa_it and target_entdaa_it codes for the ENTDAA command to work. I had only loaded controller_entdaa_it. The problem is solved now.