IBIS model STM32F765 no output
Hi, I have problem to generate correct output waveforms with Altium SI tool using the IBIS model stm32f765_767_777_lqfp144.ibs.
I'm trying to generate a clock output signal in PB3 configured as SPI1, no pulls, fast speed or high speed but the result will only be noise. I'm not sure which output model to use, there are a lot of different to select among. Think I have tried all possible models but the result will just be noise.
Example using output model io8p10_arsudq_ft_tp_out.mac:

Some of the models will generate output, but are with wrong voltage levels and are not correct one to use in my setup. Example output model io8usb_fs_otg_ft_dpdn_pupu2_st_out.mac:

I would appreciate any help with this issue to come further.