IBIS model STM32H5
I'm using STM32H573IIK6TR and I download its IBIS simulation model from st.com [stm32h562_563_573_ufbga201.ibs]
There are a lot of pin model, but i cannot understand what is the correlaction between the datasheet and ibis model.
For example:
I'm using pin H14 as SDCLK in high speed mode.
In IBIS model pins have the following models: low speed (io8_ft_spi_ls_3v3), medium speed (io8_ft_spi_ms_3v3), fast speed (io8_ft_spi_fs_3v3) and high speed (io8_ft_spi_hs_3v3).
In datasheet there are 4 mode: low, medium, high and very high.
So, I think that "high mode" in datasheet correspond to "fast speed" in IBIS model, but results don't correspond at all.