IEC60335 SelfTestLib
In our legacy STM32f103 project a ST library named "Self Test Library" is used. It has version 1.0, dated 10/01/2007. That library is certified according to IEC60335. I found it in an archive named IEC60335.zip, but I have no idea if that's the original archive name. Source files are named "stm32f10x_STL*.h/.c.
Is the library still maintained?
Can the original archive be downloaded somewhere?
Are newer versions available?