Skip to main content
Explorer II
September 5, 2024
Question

Impossible to receive data in loop using SPI with interupt

  • September 5, 2024
  • 4 replies
  • 1334 views

Hello,

I'm working with two F4 STM32 boards using the SPI communication.

The two boards are connect to each other using the SPI1 connectivity. The first board is configured as a Master and only send data. And the second is configured as a Slave and only receive data. The Baude Rate of the master is set to 656KBits/s. I disable the Hardware NSS Signal.  And the rest of the configuration is left as default.

My problem with my code is that I only get data with one iteration. The callBack function is just called once. For information, I used the exact code using DMA, by just replacing HAL_SPI_Receive_IT() by HAL_SPI_Receive_DMA(), and it works. 

This is the code I use for transfering the data   

 

///////////////////////////////////////////////
Master Transmiter 
///////////////////////////////////////////////
#define message_tx_size 4
uint8_t message_tx[message_tx_size] = "ABCD";
....
int main(void){
	while (1){
		HAL_SPI_Transmit(&hspi1, message_tx, message_tx_size, HAL_MAX_DELAY);
		HAL_Delay(100);
	}
}

and this is the code I use for receiving

///main.c Receiver SPI Interupt////

#include "main.h"
#include "string.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

ETH_TxPacketConfig TxConfig;
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */

ETH_HandleTypeDef heth;

SPI_HandleTypeDef hspi1;

UART_HandleTypeDef huart3;

PCD_HandleTypeDef hpcd_USB_OTG_FS;

/* USER CODE BEGIN PV */
volatile int msgReceved = 0;

struct Struct_Formatted_Data struct_formatted_data_rx;
int size_of_struct_formatted_data = sizeof(struct Struct_Formatted_Data);
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ETH_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_USB_OTG_FS_PCD_Init(void);
static void MX_SPI1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ETH_Init();
 MX_USART3_UART_Init();
 MX_USB_OTG_FS_PCD_Init();
 MX_SPI1_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
	 if (1 == msgReceved){ //Process the message
			msgReceved = 0;
			HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_7);
	 } else if (0 == msgReceved){
			msgReceved = -1;

			HAL_SPI_Receive_IT(&hspi1, (uint8_t *)&struct_formatted_data_rx, size_of_struct_formatted_data);
			memset(&struct_formatted_data_rx, '\0', size_of_struct_formatted_data);
	 }

	 HAL_Delay(200);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ETH Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ETH_Init(void)
{

 /* USER CODE BEGIN ETH_Init 0 */

 /* USER CODE END ETH_Init 0 */

 static uint8_t MACAddr[6];

 /* USER CODE BEGIN ETH_Init 1 */

 /* USER CODE END ETH_Init 1 */
 heth.Instance = ETH;
 MACAddr[0] = 0x00;
 MACAddr[1] = 0x80;
 MACAddr[2] = 0xE1;
 MACAddr[3] = 0x00;
 MACAddr[4] = 0x00;
 MACAddr[5] = 0x00;
 heth.Init.MACAddr = &MACAddr[0];
 heth.Init.MediaInterface = HAL_ETH_RMII_MODE;
 heth.Init.TxDesc = DMATxDscrTab;
 heth.Init.RxDesc = DMARxDscrTab;
 heth.Init.RxBuffLen = 1524;

 /* USER CODE BEGIN MACADDRESS */

 /* USER CODE END MACADDRESS */

 if (HAL_ETH_Init(&heth) != HAL_OK)
 {
 Error_Handler();
 }

 memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig));
 TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM | ETH_TX_PACKETS_FEATURES_CRCPAD;
 TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC;
 TxConfig.CRCPadCtrl = ETH_CRC_PAD_INSERT;
 /* USER CODE BEGIN ETH_Init 2 */

 /* USER CODE END ETH_Init 2 */

}

/**
 * @brief SPI1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_SPI1_Init(void)
{

 /* USER CODE BEGIN SPI1_Init 0 */

 /* USER CODE END SPI1_Init 0 */

 /* USER CODE BEGIN SPI1_Init 1 */

 /* USER CODE END SPI1_Init 1 */
 /* SPI1 parameter configuration*/
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_SLAVE;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES_RXONLY;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 10;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI1_Init 2 */

 /* USER CODE END SPI1_Init 2 */

}

/**
 * @brief USART3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART3_UART_Init(void)
{

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 huart3.Instance = USART3;
 huart3.Init.BaudRate = 115200;
 huart3.Init.WordLength = UART_WORDLENGTH_8B;
 huart3.Init.StopBits = UART_STOPBITS_1;
 huart3.Init.Parity = UART_PARITY_NONE;
 huart3.Init.Mode = UART_MODE_TX_RX;
 huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart3.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */

}

/**
 * @brief USB_OTG_FS Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USB_OTG_FS_PCD_Init(void)
{

 /* USER CODE BEGIN USB_OTG_FS_Init 0 */

 /* USER CODE END USB_OTG_FS_Init 0 */

 /* USER CODE BEGIN USB_OTG_FS_Init 1 */

 /* USER CODE END USB_OTG_FS_Init 1 */
 hpcd_USB_OTG_FS.Instance = USB_OTG_FS;
 hpcd_USB_OTG_FS.Init.dev_endpoints = 4;
 hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL;
 hpcd_USB_OTG_FS.Init.dma_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED;
 hpcd_USB_OTG_FS.Init.Sof_enable = ENABLE;
 hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.lpm_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.vbus_sensing_enable = ENABLE;
 hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE;
 if (HAL_PCD_Init(&hpcd_USB_OTG_FS) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USB_OTG_FS_Init 2 */

 /* USER CODE END USB_OTG_FS_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, LD1_Pin|LD3_Pin|LD2_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : USER_Btn_Pin */
 GPIO_InitStruct.Pin = USER_Btn_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(USER_Btn_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : LD1_Pin LD3_Pin LD2_Pin */
 GPIO_InitStruct.Pin = LD1_Pin|LD3_Pin|LD2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : USB_PowerSwitchOn_Pin */
 GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : USB_OverCurrent_Pin */
 GPIO_InitStruct.Pin = USB_OverCurrent_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

and this is for the callBack

///STM32f4_it.c Receiver SPI Interupt////
/**
 * @brief This function handles SPI1 global interrupt.
 */
void SPI1_IRQHandler(void)
{
 /* USER CODE BEGIN SPI1_IRQn 0 */

 /* USER CODE END SPI1_IRQn 0 */
 HAL_SPI_IRQHandler(&hspi1);
 /* USER CODE BEGIN SPI1_IRQn 1 */

 /* USER CODE END SPI1_IRQn 1 */
}

/* USER CODE BEGIN 1 */

 

Thank you for your help

    This topic has been closed for replies.

    4 replies

    Technical Moderator
    September 5, 2024

    @Dreamer3D wrote:

    and this is for the callBack

    ///STM32f4_it.c Receiver SPI Interupt////
    /**
     * @brief This function handles SPI1 global interrupt.
     */
    void SPI1_IRQHandler(void)
    {
     /* USER CODE BEGIN SPI1_IRQn 0 */
    
     /* USER CODE END SPI1_IRQn 0 */
     HAL_SPI_IRQHandler(&hspi1);
     /* USER CODE BEGIN SPI1_IRQn 1 */
    
     /* USER CODE END SPI1_IRQn 1 */
    }
    
    /* USER CODE BEGIN 1 */

     

    Thank you for your help


    This is not the callback, this is the SPI1 IRQ handler. The callback HAL_SPI_RxCpltCallback() is called elsewhere in HAL_SPI_IRQHandler() which I don't see in your code. 

    msgReceved needs to be set in the callback and checked/reset in your main for synchronization.

    Dreamer3DAuthor
    Explorer II
    September 5, 2024

    This is the full code from stm32f4xx_hal.c

    The callback function is on the last raws

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file stm32f4xx_it.c
     * @brief Interrupt Service Routines.
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    #include "stm32f4xx_it.h"
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN TD */
    
    /* USER CODE END TD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    /* USER CODE BEGIN PV */
    
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    /* USER CODE END 0 */
    
    /* External variables --------------------------------------------------------*/
    extern SPI_HandleTypeDef hspi1;
    /* USER CODE BEGIN EV */
    extern volatile int msgFromBouee;
    extern SPI_HandleTypeDef hspi1;
    /* USER CODE END EV */
    
    /******************************************************************************/
    /* Cortex-M4 Processor Interruption and Exception Handlers */
    /******************************************************************************/
    /**
     * @brief This function handles Non maskable interrupt.
     */
    void NMI_Handler(void)
    {
     /* USER CODE BEGIN NonMaskableInt_IRQn 0 */
    
     /* USER CODE END NonMaskableInt_IRQn 0 */
     /* USER CODE BEGIN NonMaskableInt_IRQn 1 */
     while (1)
     {
     }
     /* USER CODE END NonMaskableInt_IRQn 1 */
    }
    
    /**
     * @brief This function handles Hard fault interrupt.
     */
    void HardFault_Handler(void)
    {
     /* USER CODE BEGIN HardFault_IRQn 0 */
    
     /* USER CODE END HardFault_IRQn 0 */
     while (1)
     {
     /* USER CODE BEGIN W1_HardFault_IRQn 0 */
     /* USER CODE END W1_HardFault_IRQn 0 */
     }
    }
    
    /**
     * @brief This function handles Memory management fault.
     */
    void MemManage_Handler(void)
    {
     /* USER CODE BEGIN MemoryManagement_IRQn 0 */
    
     /* USER CODE END MemoryManagement_IRQn 0 */
     while (1)
     {
     /* USER CODE BEGIN W1_MemoryManagement_IRQn 0 */
     /* USER CODE END W1_MemoryManagement_IRQn 0 */
     }
    }
    
    /**
     * @brief This function handles Pre-fetch fault, memory access fault.
     */
    void BusFault_Handler(void)
    {
     /* USER CODE BEGIN BusFault_IRQn 0 */
    
     /* USER CODE END BusFault_IRQn 0 */
     while (1)
     {
     /* USER CODE BEGIN W1_BusFault_IRQn 0 */
     /* USER CODE END W1_BusFault_IRQn 0 */
     }
    }
    
    /**
     * @brief This function handles Undefined instruction or illegal state.
     */
    void UsageFault_Handler(void)
    {
     /* USER CODE BEGIN UsageFault_IRQn 0 */
    
     /* USER CODE END UsageFault_IRQn 0 */
     while (1)
     {
     /* USER CODE BEGIN W1_UsageFault_IRQn 0 */
     /* USER CODE END W1_UsageFault_IRQn 0 */
     }
    }
    
    /**
     * @brief This function handles System service call via SWI instruction.
     */
    void SVC_Handler(void)
    {
     /* USER CODE BEGIN SVCall_IRQn 0 */
    
     /* USER CODE END SVCall_IRQn 0 */
     /* USER CODE BEGIN SVCall_IRQn 1 */
    
     /* USER CODE END SVCall_IRQn 1 */
    }
    
    /**
     * @brief This function handles Debug monitor.
     */
    void DebugMon_Handler(void)
    {
     /* USER CODE BEGIN DebugMonitor_IRQn 0 */
    
     /* USER CODE END DebugMonitor_IRQn 0 */
     /* USER CODE BEGIN DebugMonitor_IRQn 1 */
    
     /* USER CODE END DebugMonitor_IRQn 1 */
    }
    
    /**
     * @brief This function handles Pendable request for system service.
     */
    void PendSV_Handler(void)
    {
     /* USER CODE BEGIN PendSV_IRQn 0 */
    
     /* USER CODE END PendSV_IRQn 0 */
     /* USER CODE BEGIN PendSV_IRQn 1 */
    
     /* USER CODE END PendSV_IRQn 1 */
    }
    
    /**
     * @brief This function handles System tick timer.
     */
    void SysTick_Handler(void)
    {
     /* USER CODE BEGIN SysTick_IRQn 0 */
    
     /* USER CODE END SysTick_IRQn 0 */
     HAL_IncTick();
     /* USER CODE BEGIN SysTick_IRQn 1 */
    
     /* USER CODE END SysTick_IRQn 1 */
    }
    
    /******************************************************************************/
    /* STM32F4xx Peripheral Interrupt Handlers */
    /* Add here the Interrupt Handlers for the used peripherals. */
    /* For the available peripheral interrupt handler names, */
    /* please refer to the startup file (startup_stm32f4xx.s). */
    /******************************************************************************/
    
    /**
     * @brief This function handles SPI1 global interrupt.
     */
    void SPI1_IRQHandler(void)
    {
     /* USER CODE BEGIN SPI1_IRQn 0 */
    
     /* USER CODE END SPI1_IRQn 0 */
     HAL_SPI_IRQHandler(&hspi1);
     /* USER CODE BEGIN SPI1_IRQn 1 */
    
     /* USER CODE END SPI1_IRQn 1 */
    }
    
    /* USER CODE BEGIN 1 */
    void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi) {
    	if(hspi->Instance == hspi1.Instance && -1 == msgReceved ) {
    		 msgReceved = 1;
    	}
    
    }
    /* USER CODE END 1 */
    Super User
    September 5, 2024

    Duplicate or same issue?

    \0 is added in the front of my message when using ... - STMicroelectronics Community

    Seems like you had it working better than this before. What did you change?

     

    Almost certainly what is happening is your master is sending data too fast and the slave has a data overrun (OVR flag), which stops it from receiving new data.

    It is important to understand how SPI communication works and to ensure the slave is ready to receive data prior to the master sending data. You don't seem to have any synchronization mechanism to get the two on the same page, or any mechanism for the slave to signal to the master that it is ready to send data. You have a delay of 200 ms which is no doubt causing issues.

    Dreamer3DAuthor
    Explorer II
    September 5, 2024

    I have two different problems :

    1) I can receive data from the transmiter when using DMA, but not with Interupt, using the exact code

    2) When I receive data using DMA, the data is alterd, an '\0' added at the begening of my message. This happens after two itteration inside the loop. I resolved the problem by reinitialize the DMA and the SPI every iteration. But this solution seems not be good according to @BarryWhit    

     

    I have 200ms delay before resending the data on the transmiter side

    Technical Moderator
    September 5, 2024

    @Dreamer3D wrote:

    Hello,

    I'm working with two F4 STM32 boards using the SPI communication.


    Also you can refer to that example: a SPI communication in full duplex between two F4 boards (using HAL_SPI_TransmitReceive_IT()):

    https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F4-Discovery/Examples/SPI/SPI_FullDuplex_ComIT

    Graduate II
    September 5, 2024

    @Dreamer3D, please pick one thread and stick to it.