Inconsistency Error during In-Application Firmware Update on STM32H7
Hello everyone,
I'm working on an in-application firmware update for an STM32H7 series microcontroller. The process involves erasing and then writing to the flash memory. I can successfully erase bank 2, but I'm encountering an issue when writing to the flash.
Issue Description: After the first 256 bits (flash-word) are written without any error, the subsequent write operations result in an inconsistency error. Interestingly, even though the HAL_FLASH_Program function returns an error, when I compare the write buffer with the flash memory, all the data appears to have been written correctly.
Code Snippet:
HAL_StatusTypeDef flash_write(uint32_t address, uint8_t* data, size_t size) { HAL_StatusTypeDef status = HAL_OK; HAL_FLASH_Unlock(); for (size_t i = 0; i < size; i += 8) { if (address + i <= (FLASH_END_ADDRESS - 8)) { status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, address + i, (uint32_t )data + i); // if (status != HAL_OK) { // break; // Exit if there's an error // } // Verify the content of flash with RAM if (*(uint32_t*)(address + i) != *(uint32_t*)(data + i)) { status = HAL_ERROR; // Set an error status if verification fails break; } else { status = HAL_OK; } } else { status = HAL_ERROR; // Set an error status if out of bounds break; } } HAL_FLASH_Lock(); return status; }
Observations:
- The first write operation succeeds, but subsequent ones return an error despite the data being written correctly.
- I've included a verification step after writing each 256-bit flash-word, which confirms that the data in flash matches the data in the RAM.
Questions:
- Has anyone encountered a similar issue with the STM32H7 series or other STM32 series?
- Could this be a known issue with the HAL library or something related to the specific flash memory behavior?
- Are there any recommended steps or checks to perform when encountering such inconsistencies?
Any insights or suggestions would be greatly appreciated!