Init Ethernet on STM32H7 error
Hi, I'm trying to create my first project with ethernet on STM32H7. I tried to give an example with a nulceo with a similar chip and I succeeded, now I'm moving on to my custom board.
I configured the system with STM32CubeIDE, generated the code and just tried to launch the program, what happens is that during initialization, at this point:
/* Dummy read to sync with ETH */
(void)SYSCFG->PMCR;
/* Ethernet Software reset */
/* Set the SWR bit: resets all MAC subsystem internal registers and logic */
/* After reset all the registers holds their respective reset values */
SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR);
/* Get tick */
tickstart = HAL_GetTick();
/* Wait for software reset */
while (READ_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR) > 0U)
{
if (((HAL_GetTick() - tickstart) > ETH_SWRESET_TIMEOUT))
{
/* Set Error Code */
heth->ErrorCode = HAL_ETH_ERROR_TIMEOUT;
/* Set State as Error */
heth->gState = HAL_ETH_STATE_ERROR;
/* Return Error */
return HAL_ERROR;
}
}
I get the return HAL_ERROR; error and the program stops.
Can you help me understand where the problem is?
I attach the ioc file that I used to generate the code, if you think the problem may be in the hardware part, I can also send the electrical diagram and layout.
Thanks in advance.
IOC File: https://drive.google.com/file/d/1BTQGlH5RxBeBbijaUmBP7SGDBpZXNBO-/view?usp=drive_link