Input capture not detecting square wave
I have built a sine wave to square wave circuit and now want to measure its frequency with the STM. I can see on the oscilloscope that the circuit works, however I can detect neither a rising nor a falling edge with the chip. It is not a problem with the code as I can detect both when they are generated by the chip with PWM or externally with a generator (which is old and its square wave really isn't that square) but also they are much slower.
The frequency of the wave is 1.24MHz, measured with the oscilloscope. I don't think that this is too fast, the timer runs at 96Mhz, but maybe using interrupts at this speed is too much?
The minimum voltage of the wave is 0.6V. I am suspecting that might be too high to be considered a logical 0 but I can't find documentation.
I would appreciate any input and also if you could point me to documentation that would be nice!