Input impedance of the STM32H735 AD converter
Hello everyone.
I am currently considering using the STM32H735 AD converter.
As shown in the figure, I have inserted a Schottky barrier diode and a 1kΩ resistor just before the ADC terminal pin for overvoltage protection.
I was curious about the input impedance of the ADC pin, so I read the specifications, and I was wondering if RAIN corresponds to the input impedance? I will be using a 12-bit ADC, so in this case, will the impedance be MAX
680Ω? If so, the signal level will drop, so I will have to reconsider the protection circuit.
・What is the input impedance of the ADC pin?
・If you are actually using this microcontroller, what type of protection circuit do you use?
I would appreciate your advice.