input resistance of a trigger pin
Hi,
I wan't to use the stm32 as described in the video
https://controllerstech.com/stm32-timers-9-one-pulse-mode/
with the difference that I uses the trm4 and the input trigger is channel 1.
Operation is ok but applying the signal from a 3.3v signal generator lowers it to 2.3v! It's as if the input resistance of the trigger was a little too low. But I can't find anything about this. I applied this same signal to an input on capture, and there no problem, the signal remains at 3.3v.
Do you have any idea about the cause of this drop in signal?
Michel