Skip to main content
Visitor II
July 13, 2024
Solved

Inquiry about- DCMI of STM32U595RJT6Q

  • July 13, 2024
  • 2 replies
  • 850 views

Good Evening Sir/Mam, 

Sir/Mam, I have a query about the DCMI of STM32U595RJT6Q. I have read the Datasheet of STM32U595xxx and it was written in it that- DCMI of this MCU is for use with Black & White Camera Modules and it is assumed that all preprocessing is pre- performed in the Camera Module. 

Sir/Mam, it would be very helpful if you could please confirm and verify these both things (Interface with Black & White Camera Module and Preprocessing is needed to be pre-  performed in the Camera Module), and if you could please provide any-  websites at which- X24 & X5 Camera Modules would be available at cheapest rates (if any). 

 

Thanking You, 

ANKUR. 

    This topic has been closed for replies.
    Best answer by KDJEM.1

    Hello @Ankur_1 and welcome to the community :),

     

    The DCMI interface is not supported in the STM32U595RJT6Q, but is supported in the STM32U595RJT6 as mentioned in the datasheet. 

    KDJEM1_0-1721032148798.png

    KDJEM1_1-1721032182842.pngKDJEM1_2-1721032233588.png

    According to this sentence "This interface is for use with black and white cameras, X24 and X5 cameras, and it is
    assumed that all preprocessing such as resizing is performed in the camera module."

    In fact X5 and X24 cameras are referring to very old ST cameras and should be removed from the datasheet to avoid any confusion with updated X24 cameras that can be found on internet. I reported this internally.

    To know if a CMOS sensor (a camera module) is compatible with the DCMI or not, the user must check the
    following points in the CMOS sensor specifications:
    • parallel interface (8-, 10-, 12-, or 14-bit)
    • control signals (VSYNC, HSYNC, and PIXCLK)
    • supported pixel clock frequency output
    • supported data output

    AN5020 application note mentioned some CMOS sensors examples that are compatible with the STM32 DCMI.

    KDJEM1_3-1721032630931.png

    Internal ticket number: 186544 (This is an internal tracking number and is not accessible or usable by customers).

    Thank you.

    Kaouthar

     

    2 replies

    KDJEM.1Answer
    Technical Moderator
    July 15, 2024

    Hello @Ankur_1 and welcome to the community :),

     

    The DCMI interface is not supported in the STM32U595RJT6Q, but is supported in the STM32U595RJT6 as mentioned in the datasheet. 

    KDJEM1_0-1721032148798.png

    KDJEM1_1-1721032182842.pngKDJEM1_2-1721032233588.png

    According to this sentence "This interface is for use with black and white cameras, X24 and X5 cameras, and it is
    assumed that all preprocessing such as resizing is performed in the camera module."

    In fact X5 and X24 cameras are referring to very old ST cameras and should be removed from the datasheet to avoid any confusion with updated X24 cameras that can be found on internet. I reported this internally.

    To know if a CMOS sensor (a camera module) is compatible with the DCMI or not, the user must check the
    following points in the CMOS sensor specifications:
    • parallel interface (8-, 10-, 12-, or 14-bit)
    • control signals (VSYNC, HSYNC, and PIXCLK)
    • supported pixel clock frequency output
    • supported data output

    AN5020 application note mentioned some CMOS sensors examples that are compatible with the STM32 DCMI.

    KDJEM1_3-1721032630931.png

    Internal ticket number: 186544 (This is an internal tracking number and is not accessible or usable by customers).

    Thank you.

    Kaouthar

     

    Technical Moderator
    October 15, 2025

    Hello @Ankur_1 ;

     

    The issue is fixed in the datasheet DS13633 Rev3.

     

    Thank you.

    Kaouthar