Inquiry about the- DCMI of STM32U5 Series MCUs.
Good Afternoon Sir/Mam,
Sir/Mam, I have a query about the DCMI of STM32U5 Series MCUs. I have read the Datasheet of following MCUs-
1) STM32U5A5VJT6Q
2) STM32U595VJT6
3) STM32U595ZJT6Q
4) STM32U5A5AJH6
5) STM32U5A5QJI6Q
6) STM32U5A9NJH6Q
7) STM32U5A9ZJT6Q
8) STM32U599VJT6
9) STM32U5G9NJH6Q
10) STM32U5G9VJT6Q
11) STM32U5G9ZJT6Q
, and, it was written in them that- DCMI of these MCUs is for use with Black & White Camera Modules Only and it is assumed that all preprocessing is pre- performed in the Camera Module.
Sir/Mam, it would be very helpful if you could please confirm and verify these both things (Interface with Black & White Camera Modules only and Preprocessing is needed to be pre- performed in the Camera Module), and if you could please provide any- websites at which- X24 & X5 Camera Modules would be available at cheapest rates (if any).
Thanking You,
ANKUR.