Interfacing STM32F429VIT6 with TFT LCD display without using external RAM
Hi ST community,
Recently i am working on a project, home automation, and i would like to use STM32F429VIT6 MCU and 3.5 inch 320RGB x 480 LCD display on the project. The LCD display controller is ST7365P from Sitronix, with Frame Memory Size: 320 x 480 x 18-bit = 2,764,800 bits.
My question is, is it possible to interface STM32F429VIT6 MCU with the TFT-LCD display through LTDC without using an external RAM just by using the On-chip Frame Memory?
Attached are the TFT-LCD display and the ST7365 controller datasheet.
Regards,