Interrupt callback only work when hitting debug break point
Hi, I was trying to implement timer interrupt on an ST32F407 Discovery board. The ST-Link on my board has been broken so I used an external ST-Link dongle and I have it connected by following this post:
I set up the timer so it will trigger interrupt once every 1s, but when I upload the code it does not go into interrupt. Only when I debug and put a break point in the callback function that it can execute the interrupt.
Here is a link to my code:
https://github.com/datcamap/DISCOVERYstm32.git
Callback function