Interrupt for Output Compare no Output does not trigger - Need diagnostics
I have TIM20 configured in reset mode with CH1 as the trigger. I want an interrupt to run if the counter reaches a certain value. I’m using CubeIDE with CH2 configured with Output Compare no Output and the pulse duration set to the desired compare value. None of the other channels are used. I haven't used output compare features before and I'm likely missing something simple.
I’m not seeing the interrupt run. I can see an input square wave on my scope. If dump TIM20->CNT to the DAC I can see it count up and reset on the edges as expected. The ramp crosses the capture compare value, so I know the value is being hit, but I don't see the interrupt trigger.
When using Cube Programmer to read the registers:
I see TIM20-> DIER CC2IE bit is set.
I see TIM20->SR CC2IF set to 0 and all the other CCxIF bits set to 1. I clear CC2IF in the interrupt so it makes sense its clear, but why would the others be set?
I start TIM20 with the following lines:
HAL_TIM_Base_Start_IT(&htim20);
HAL_TIM_OC_Start_IT(&htim20,TIM_CHANNEL_2);
This is my interrupt code:
TIM20_IT_CNT++;
DAC1->DHR12R2 = (TIM20->CNT%2)*0xFFF; //generates square wave for observable output
TIM20->SR &= 0xFFFFFFFB; //resets the interrupt flag
IOC attached
What am I doing wrong?