Is is possible to wakeup the STM32L496 with an external interrupt in standby mode
Hello,
currently I'm using stm32l496 in that i want to wake up the controller from the standby mode on an external interrupt.
i configured pin PC13 (supports wake up functionality) as an external interrupt with rising edge , now when the MCU enters into the standby mode, upon receiving external interrupt will the device wakeup?