Is it a bug? STM32F0xx HAL USART Driver
Hello All,
I am using USART peripheral to transfer a block of bytes. I am trying to do it using DMA. Because I want all bytes of USART frame should be dispatched without any gaps between them and my system has few interrupts that could bring gaps between the byte if I transfer using polling mode.
So I have configured the DMA channel for this. But my problem is that DMA Transfer complete Callback is not getting invoked by HAL Driver. I am using Normal DMA mode and NOT the circular mode.
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
when I debugged the code I found that the HAL driver file stm32f0xx_hal_uart.c file line no 3533
static void UART_DMATransmitCplt(DMA_HandleTypeDef *hdma)
is only invoking the HAL_UART_TxCpltCallback() when the DMA type is Circular (see the screenshot below) so is it a bug? Because HAL documentation doesn't state that the callback will be called only for CIRCULAR mode and NOT normal more. Nor does this code is making any sense.

When I removed the "else" keyword, my callback is getting called. I have also referred to a previous version of the HAL driver, there also the logic is same and also in STM32F4's HAL driver.