Question
Is there any STM32 MCU which has ADC with range higher than 3.3V ?
I want to monitor my 4.2V battery and cant find any MCU which can convert such high voltage . It will be even better if it has differential ADC [can do 1.5-4.5].Previously tries STM32F303C8T6 but all the ADC pins are only 3.3V Tolerant. Its my first time posting so really don't know if i'm posting in the right page.