Is VREF+ pin required to be connected if VREFBUF is configured as an internal reference on STM32G4?
I began using an STM32G473 and the DAC outputs are acting funny. I have VREFBUF configured as an internal reference. Since I'm not using VREF+ as an output, I left the pin unconnected. I posted a thread about it and it was recommended that I connect VREF+ through a cap to ground. I'm working with a custom board where this isn't possible so I can't test.
I haven't found anything in the documentation that would suggest leaving the VREF+ pin unconnected would have ill effects on DAC outputs. Is this documented anywhere?
Original thread: