Issue with SDIO Initialization Causing MCU Communication Failure on Custom STM32H747 Board
Dear sir,
In our custom board, we are using the STM32H747XIH6 microcontroller with Wi-Fi functionality. The Wi-Fi module part number is LBEE5KL1DX-883, and it is connected via the SDIO interface.
We have properly configured the I/O pins in STM32CubeMX and generated the code. However, once the SDIO initialization is executed, we are unable to communicate with the MCU.
Without SDIO initialization, the board works fine.
Could you please help us identify the issue?
Best regards,
Samudralnakaiah.