Skip to main content
Visitor II
March 10, 2025
Question

Issue with USB Power Delivery Sink on STM32 - ERROR with Trace_Notif :78

  • March 10, 2025
  • 1 reply
  • 894 views

Hi everyone,

I’ve been following the official ST guide for setting up USB Power Delivery (PD) Sink on an STM32 device, as outlined here: Getting started with USB-Power Delivery Sink.

I successfully compiled and flashed the firmware onto my NUCLEO-G071RB board. When I tried connecting my setup (NUCLEO-G071RB + X-NUCLEO-SNK1M1) to an external monitor via USB-C to test the power delivery negotiation, I encountered an issue: `ERROR with Trace_Notif :78`.

The issue can be caught when debugging using STM32CubeMonitor-UCPD.
I've attached the whole trace.

Kind regards,
Vlado

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    March 26, 2025

    Hi @vladovlado 

    Would you attach your test case to reproduce the issue on my end?

    Visitor II
    March 26, 2025

    Hi @FBL 

    Here is the zip of the whole project + traces with another source device.
    The ERROR happens when I plug the cable from laptop/monitor to snk1m1.

    Update on the project:
    The PD part works, but the source of the ERROR trace is still unknown. The error message is some kind of a timeout but the question remains, why does it trigger?

    Also, I would kindly ask you to review https://community.st.com/t5/stm32-mcus-embedded-software/vdm-issue-pe-send-notsupported-on-stm32g071rb-snk1m1-sink-mode/td-p/786718
    since it's the same hardware.

    Kind regards,
    Vlado

    Graduate II
    April 15, 2025

    I am also getting this error using an STM32G0B1 with a TCPP03-M20.

    NMartin_1-1744756930601.png