Issues using CMSIS Inverse FFT on STM32
Hey everyone. I am working on a project where I am attempting to detect a frequency of a signal using autocorrelation. I am doing this through applying FFTs and IFFTs. Basically, I have been running into some issues trying to get the correct functionality using the CMSIS dsp library and I am really struggling to figure out what is wrong and how to correct it. To provide proof of concept, I first implemented the algorithm in python like so:
def autocorrelation_via_fft(x):
# Compute the FFT and then (its magnitude)^2
Fx = np.fft.fft(x)
Pxx = np.abs(Fx)**2
# Inverse FFT to get autocorrelation
autocorrelation = np.fft.ifft(Pxx)
autocorrelation = np.real(autocorrelation)
return autocorrelation[:len(x)//2]
And this works very well for getting an autocorrelation result and combined with some peak detection, I can very accurately determine the frequency being play with harmonics (in my case a guitar). I then proceeded to translate this code into C using the FFTW library like so:
void autocorrelate(double* x, int N, double* autocorrelation) {
// Allocate input and output arrays for the FFT
fftw_complex *in, *out;
in = (fftw_complex*) fftw_malloc(sizeof(fftw_complex) * N);
out = (fftw_complex*) fftw_malloc(sizeof(fftw_complex) * N);
// Copy the real signal into the complex input array
for (int i = 0; i < N; i++) {
in[i][0] = x[i]; // Real part
in[i][1] = 0.0; // Imaginary part
}
// Create a plan to calculate the FFT of the signal
fftw_plan plan_forward = fftw_plan_dft_1d(N, in, out, FFTW_FORWARD, FFTW_ESTIMATE);
// Execute the plan to calculate the FFT
fftw_execute(plan_forward);
// Calculate the power spectrum (magnitude squared of the FFT)
for (int i = 0; i < N; ++i) {
double real = out[i][0];
double imag = out[i][1];
out[i][0] = real * real + imag * imag; // Magnitude squared
out[i][1] = 0.0; // Zero out the imaginary part since it should not affect the result
}
// Create a plan to calculate the inverse FFT of the power spectrum
fftw_plan plan_backward = fftw_plan_dft_1d(N, out, in, FFTW_BACKWARD, FFTW_ESTIMATE);
// Execute the plan to calculate the inverse FFT
fftw_execute(plan_backward);
// Copy the real part of the inverse FFT result into the autocorrelation array
for (int i = 0; i < N; ++i) {
autocorrelation[i] = in[i][0] / N; // Scale result by N for proper normalization
}
// Free the memory allocated for the FFTW arrays and plans
fftw_destroy_plan(plan_forward);
fftw_destroy_plan(plan_backward);
fftw_free(in);
fftw_free(out);
}
And this produces the exact same result for autocorrelation as python using the FFTW dsp functions (although I had to do more conditioning/normalizing of the data compared to python). I should note that for testing I have just been using a pure sinusoid at 82 Hz to verify functionality (python works on real audio data I confirmed).
Now that's all great, but I can not seem to get the same functionality as this C code when working on the STM32 with CMSIS and I feel like I've tried everything, so I am not certian that the ifft/fft functions in CMSIS are exactly the same as FFTW or python. Here is my (not working attempt):
void autocorrelate(float32_t* x, uint32_t N, float32_t* autocorrelation) {
float32_t* p_fft_input;
float32_t* p_fft_output;
arm_rfft_fast_instance_f32 fftInstance;
// Allocate memory for the input and output arrays
p_fft_input = (float32_t *)malloc(sizeof(float32_t) * N * 2); // FFT input is 2x for complex numbers?
p_fft_output = (float32_t *)malloc(sizeof(float32_t) * N * 2); // FFT output is also 2x for complex numbers?
// Initialize the FFT instance
arm_rfft_fast_init_f32(&fftInstance, N);
// Zero-pad the input array and copy the real signal into the input array
for (uint32_t i = 0; i < N; ++i) {
p_fft_input[i * 2] = x[i]; // Real part
p_fft_input[i * 2 + 1] = 0.0f; // Imaginary part, which is zero
}
// Calculate the FFT
arm_rfft_fast_f32(&fftInstance, p_fft_input, p_fft_output, 0);
// Calculate the power spectrum (magnitude squared)
for (uint32_t i = 0; i < N; ++i) {
arm_cmplx_mag_squared_f32(&p_fft_output[i * 2], &p_fft_output[i], 1);
}
// Inverse FFT to get autocorrelation
arm_rfft_fast_f32(&fftInstance, p_fft_output, autocorrelation, 1);
// Normalize
for (uint32_t i = 0; i < N; ++i) {
autocorrelation[i] /= (float32_t)N;
}
free(p_fft_input);
free(p_fft_output);
}
I tried to implement sort of what FFTW is doing, but I am not sure if that is right. But regardless, what I should get for the autocorrelation is
Autocorrelation:
767.814944
761.705596
743.474793
713.412709
671.997833
....
I instead get very off numbers:

I am very stuck on this, so if anyone has any sort of insight as to why the cmsis library is not producing similar results I would appreciate. I am thinking I might have to do more conditioning to the input to the ifft due to some differences, but what that is I am not sure. I pretty much only have a basic understanding of how these functions work.
Thanks.