Issues with FM24CLXX_WriteData function in STM32 project
I have the following function to write data to the FM24CL64 memory:
void FM24CLXX_WriteData(uint16_t memAddr, uint8_t *data, uint16_t size) {
uint8_t memAddrData[2] = { (uint8_t)(memAddr >> 8), (uint8_t)(memAddr & 0xFF) };
HAL_StatusTypeDef status = HAL_I2C_Mem_Write(&hi2c1, FM24CLXX_I2C_ADDR, memAddrData[0], I2C_MEMADD_SIZE_8BIT, data, size, 100);
if (status != HAL_OK) {
Error_Handler();
}
}
Symptoms:
- The write operation fails, but the HAL_StatusTypeDef status returns a code that doesn't indicate exactly where the issue is.
- I have verified that the I2C address FM24CLXX_I2C_ADDR = 0xA0 is correct.
- The Error_Handler() function is being triggered, but I don't know exactly why.
Possible Causes:
- There could be an issue with how the I2C command is sent.
- Maybe the address or size format isn't compatible with the memory or STM32 I2C configuration.
Request:
- Anyone with experience in using STM32 with I2C and FM24CLXX memory, could you please help me identify what could be wrong?
- Suggestions for debugging or best practices when working with I2C memory like the FM24CL64 would be appreciated.
Full code:
This is my full code, I using stm32f405 OpenX05R-C board.
#include "main.h"
#include "cmsis_os.h"
#include <stdio.h>
#include "backup_sram.h"
#include "fm24clxx.h"
#define Avg_slope (2.5F)
#define V_25 (0.76F)
osThreadId_t Task1Handle;
osThreadId_t Task2Handle;
osThreadId_t Task3Handle;
osMutexId_t sharedMutex;
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart2;
// Printf with USART
int _write(int file, char *data, int len) {
HAL_UART_Transmit(&huart2, (uint8_t*)data, len, HAL_MAX_DELAY);
return len;
}
uint32_t temperature_value;
volatile uint8_t button_pressed = 0;
#define DEBOUNCE_DELAY 50
#define STABLE_THRESHOLD 4
int is_button_pressed() {
uint8_t counter = 0;
uint8_t i;
uint8_t button_input;
button_input = HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_1);
if (button_input != GPIO_PIN_RESET) {
return 0;
}
for (i = 0; i < 10; i++) {
osDelay(5);
button_input = HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_1);
if (button_input == GPIO_PIN_SET) {
counter = 0;
} else {
counter++;
}
if (counter >= STABLE_THRESHOLD) {
return 1;
}
}
return 0;
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc) {
if (hadc->Instance == ADC1) {
// float value = HAL_ADC_GetValue(&hadc1);
float value = temperature_value;
float V_sense = (value * 3.0f) / 4095.0f;
temperature_value = (uint32_t)((V_sense - V_25) / Avg_slope + 25.0f);
printf("ADC value: %d, Temperature: %lu\r\n", (int)V_sense, temperature_value);
BKPSRAM_Write(0x00, temperature_value);
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_1);
}
}
void Task1_Blink_LED(void *argument) {
while (1) {
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0);
osDelay(1000);
}
}
void Task2_Read_Temperature(void *argument) {
while(1){
HAL_ADC_Start_DMA(&hadc1, &temperature_value, 1);
osDelay(5000);
uint32_t temp_from_sram = BKPSRAM_Read(0x00);
printf("Temp from Backup SRAM: %lu\r\n", temp_from_sram);
// HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_1);
}
// while (1) {
// HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_1);
// osDelay(1000);
// }
}
void Task3_Button_Check(void *argument) {
static uint8_t button_stable = 0;
while(1){
printf("t3\r\n");
if (is_button_pressed()) {
printf("0.\r\n");
if (!button_stable) {
button_stable = 1;
if (!button_pressed) {
button_pressed = 1;
uint32_t temperature;
printf("1.\r\n");
temperature = BKPSRAM_Read(0x00);
printf("2.%lu\r\n", temperature);
FM24CLXX_WriteData(0x0000, (uint8_t*)&temperature, sizeof(temperature));
printf("Button Pressed, Data written to FM24CLXX: %lu\r\n", temperature);
uint32_t read_temp;
FM24CLXX_ReadData(0x0000, (uint8_t*)&read_temp, sizeof(read_temp));
printf("Data read from FM24CLXX: %lu\r\n", read_temp);
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_2);
}
}
} else {
if (button_stable) {
button_stable = 0;
button_pressed = 0;
}
}
osDelay(10);
}
}
void RTOS_Tasks_Init() {
osThreadAttr_t task1_attr = {.name = "Task1", .priority = osPriorityNormal, .stack_size = 128 * 4};
osThreadAttr_t task2_attr = {.name = "Task2", .priority = osPriorityNormal, .stack_size = 128 * 4};
osThreadAttr_t task3_attr = {.name = "Task3", .priority = osPriorityHigh, .stack_size = 128 * 4};
Task1Handle = osThreadNew(Task1_Blink_LED, NULL, &task1_attr);
Task2Handle = osThreadNew(Task2_Read_Temperature, NULL, &task2_attr);
Task3Handle = osThreadNew(Task3_Button_Check, NULL, &task3_attr);
}
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART2_UART_Init(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_I2C1_Init();
MX_USART2_UART_Init();
BKPSRAM_Init();
sharedMutex = osMutexNew(NULL);
osKernelInitialize();
RTOS_Tasks_Init();
osKernelStart();
while (1){
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = ENABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 2;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_144CYCLES;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Rank = 2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* Enable DMA controller clock
*/
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA2_Stream0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, led0_Pin|led1_Pin|led2_Pin|led3_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : PA1 */
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pins : led0_Pin led1_Pin led2_Pin led3_Pin */
GPIO_InitStruct.Pin = led0_Pin|led1_Pin|led2_Pin|led3_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI1_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(EXTI1_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE END 4 */
/**
* @brief Period elapsed callback in non blocking mode
* @note This function is called when TIM6 interrupt took place, inside
* HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
* a global variable "uwTick" used as application time base.
* @PAram htim : TIM handle
* @retval None
*/
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
/* USER CODE BEGIN Callback 0 */
/* USER CODE END Callback 0 */
if (htim->Instance == TIM6) {
HAL_IncTick();
}
/* USER CODE BEGIN Callback 1 */
/* USER CODE END Callback 1 */
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */