Issues with STM32H7 and SPI on trasmission
Hello,
I'm just started using a nucleo-h742x. I have configured the SPI and the Fatfs library using the default settings, the SPI speed was configured at speed below 1Mbit/s. The sys clock is below 100MHz.
I always get disk_not_ready error when trying to mount the drive (error code 3).
The problem is that I don't see any signal on the MOSI line when a transaction should appear. I have also tried a simple HAL_spi_transmit(), but I have the same problem. I see the clock appearing but no signal on MOSI.
Someone has some suggestions? On other STM32 M4/M3/M0 I have no problem using the same code.