Issues writing float data to UART
Hello everyone!
Ran into some issues writing float data to the UART. I know with Nordic, there was some weird workaround that had to be used to convert it that looked something like this:
NRF_LOG_INFO("MLX90393 X = " NRF_LOG_FLOAT_MARKER "\r", NRF_LOG_FLOAT(*x));I wasn't sure if there was some other trick for this, if there's a project related setting that is required to make use of floating point (in case it's disabled by default or something to that effect, etc). I tried finding one but didn't seem to find one in the project options.
Anyway, this is my current attempt at resolving the issue:
void write_mlx90393_to_uart(float x, float y, float z)
{
x = 250.3;
y = -112.3;
z = 15.214;
char x_str[30];
char y_str[30];
char z_str[30];
sprintf(x_str, "X: %f", x);
sprintf(y_str, "Y: %05.2f \n", y);
sprintf(z_str, "Z: %05.2f \n", z);
debugPrintln(&huart1, x_str);
debugPrintln(&huart1, y_str);
debugPrintln(&huart1, z_str);
}I expected it would convert it but the output for x_str is:
"X: \0\230\0\0 \224\0\0 \204\001\a\030N\0\002\0>\a\0\030\022ÿÿÿÿÿ"
or
0x2002ffa8Had to hardcode the values in this function to even test this as the values aren't being passed to the function as I would've expected. One problem at a time though! Heh . . .
Any suggestions you guys can point me towards would be greatly appreciated. Thanks!