IWDG resetting when making the window larger
- STM32G0B0RE
Our controller was running fairly well but on occasion we were seeing the windowed watchdog trip(The IWDDGRSTF flag set on reboot.) We were not sure whether this was a too short or too long trip so decided to extend the window wider(set the Reload counter from 1800 to 2500.) The kick logic runs from the system clock and is set to reload the every 1.0 second or greater.
The original window should be running between ~781msec and 1.77 sec +/- the 32kHz clock inaccuracy. What is odd is that this work very well but on occasion would trip. But simply expanding the end of the window to 2.44 sec (~781msec to 2.44 sec) the watchdog trips frequently.
Is there some relationship between the two times that we did not understand from RM0454? Is there something wrong with the setup code below?
Thanks
void IWDG_Config(void)
{
// Source clock is the LSI(independent internal 32 kHz RC.)
// Enable IWDG (the LSI oscillator will be enabled by hardware)
LL_IWDG_Enable(IWDG);
// Enable write access to IWDG_PR and IWDG_RLR registers
LL_IWDG_EnableWriteAccess(IWDG);
// Set IWDG Prescaler value to 32. The clock is now
// 32kHz/32 = 1024Hz
LL_IWDG_SetPrescaler(IWDG, LL_IWDG_PRESCALER_32);
// Set IWDG Reload value to 1800.
// 1024 hHz has a period of 1/1024 = 0.9765msec
// // 0.9765msec * 1800 = 1.7577sec watchdog timeout
// LL_IWDG_SetReloadCounter(IWDG, 1800);
// 0.9765msec * 2500 = 2.44125sec watchdog timeout
LL_IWDG_SetReloadCounter(IWDG, 2500);
// Wait until RVU flag is reset to be sure that the reload value
// update operation is completed.
while(LL_IWDG_IsActiveFlag_RVU(IWDG) != RESET);
// Set the IWDG window value to 800.
// (0.9765msec * 800) = 781.25msec start window.
LL_IWDG_SetWindow(IWDG, 800);
// The watchdog window starts at 781msec and goes to 1.757seconds so the watchdog
// kick must happen in between these times.
// Kicked it after every 781msec but before every 1.757sec
// The WATCHDOG_KICK_COUNT is currently set to 900msec, so any changes in this function
// must be checked against this value as the main loop uses it to know when to kick the
// watchdog.
}