Skip to main content
Graduate II
October 27, 2025
Solved

L073: ADC & DMA, strange buffer "shift" in CIRCULAR mode

  • October 27, 2025
  • 11 replies
  • 472 views

Heyho,

strange things happening that I'd like to understand for a STM32L073 (Nucleo for now).

Setup on a L073 @ 32MHz:

- ADC is clocked by PCLK/4
- ADC prescaler = 2 -> divide by 4 -> 2 MHz
- 12 bit right aligned
- ref V = VDDA = 3.3V
- hardware oversampling + shift is used (great feature!)
- 7 ADC channels sequenced
- DMA, with buffer for 8 samples per channel -> u16AdcDmaBuf[56]

 

In non-circular mode (CIRC neither set in DMA- nor in AD-registers), after each DMA's transfer complete interrupt, DMA and ADC are restarted, everything is as it should be, and as it is set in the sequencing registers.

Here's what the DMA buffer looks like, and all this makes sense:
buffer[0] = 2031 is the DAC output set to 2047,
buffer[1] & buffer[2] = 4095 are connected to VDDA -> 4095 ok,
buffer[5] is internal VREF = 1.2V -> perfect,
buffer[6] is internal temperature sensor -> ~24°C -> perfect

1) ADC & DMA: not circular

DmaBuf
[00] 2031 4095 4095 1926 3083 1524 0604
[07] 2031 4095 4095 1926 3083 1524 0604
[14] 2031 4095 4095 1927 3081 1525 0604
[21] 2031 4095 4095 1925 3081 1525 0605
[28] 2031 4095 4095 1926 3081 1525 0605
[35] 2031 4095 4095 1926 3081 1525 0605
[42] 2031 4095 4095 1926 3081 1525 0605
[49] 2031 4095 4095 1926 3081 1526 0605
 DAC2 PWR5 PWR3 SNSA SNS5 REFI TMPI

registers:
ADC1->
ISR 0000000B
IER 00000000
CR 10000005
 REGEN
 START
 EN
CFGR1 = 00003001
 CONT
 OVRMOD
 right aligned
 DMAEN

DMA1_Channel1->
CCR 0000358B
 EN
 TCIE
 TEIE
 MINC
 MSIZE = 1 = 16b
 PSIZE = 1 = 16b

 

Now (all before ADC / DMA start) I turn on circular mode in ADC1->CFGR1 |= DMACFG, 
and in DMA1_Channel1->CCR |= CIRC.
And now I still get some nice AD values, but the buffer has shifted by 1, compare to above:

2) ADC & DMA: CIRCular mode

DmaBuf
[00] 0602 2031 4095 4095 1926 3085 1525
[07] 0602 2031 4095 4095 1926 3084 1525
[14] 0602 2031 4095 4095 1925 3083 1525
[21] 0602 2031 4095 4095 1927 3084 1525
[28] 0602 2031 4095 4095 1926 3084 1525
[35] 0602 2031 4095 4095 1926 3084 1525
[42] 0602 2031 4095 4095 1926 3083 1525
[49] 0602 2031 4095 4095 1926 3084 1525
 DAC2 PWR5 PWR3 SNSA SNS5 REFI TMPI

registers:
ADC1->
ISR 0000000B
IER 00000000
CR 10000005
 REGEN
 START
 EN
CFGR1 = 00002003
 CONT
 right
 12b
 DMACFG = CIRC
 DMAEN

DMA1_Channel1->
CCR 000035AB
 EN
 TCIE
 TEIE
 CIRCular
 MINC
 MSIZE = 1 = 16b
 PSIZE = 1 = 16b

 

Note: register dumps are from running application

What am I missing? Been checking all registers, DS, RM, feels like I have overseen one bit or so...

 

Thanks in advance!

    This topic has been closed for replies.
    Best answer by gbm

    In the code above you are setting ADC DMAEN and DMACFG bits BEFORE calibration. This might be the problem. Do it AFTER calibration is completed.

    11 replies

    LCEAuthor
    Graduate II
    October 28, 2025

    So here's the ADC_Init().

    With 
    ADC_CONT_OVERWR = 1
    I get the bad buffer shift.

    /* +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
    /* ADC init function
     */
    void ADC_Init(void)
    {
    	/* peripheral clock enable */
    	uint32_t u32TmpReg;
    	RCC->APB2ENR |= RCC_APB2ENR_ADC1EN;
    	u32TmpReg = ( RCC->APB2ENR & RCC_APB2ENR_ADC1EN );
    	(void)u32TmpReg;
    
    /* +++++++++++++++++++++++++++++++++++++++++++++++++++ */
    /* ADC Init */
    
    	/* reset control register */
    	ADC1->CR = 0;
    	/* clock prescaler divides by 4 */
    	ADC1_COMMON->CCR = ADC_CCR_PRESC_1;
    	/* clear interrupt status */
    	ADC1->ISR = ( ADC_ISR_EOCAL | ADC_ISR_AWD | ADC_ISR_OVR | ADC_ISR_EOSEQ |
    					ADC_ISR_EOC | ADC_ISR_EOSMP | ADC_ISR_ADRDY );
    	/* interrupts disabled */
    	ADC1->IER = 0;
    
    #if ADC_CONT_OVERWR
    	/* continuous mode, overwrite, right aligned, 12bit,
    	 *	DMA circular -> auto restart ADC
    	 */
    	ADC1->CFGR1 = ( ADC_CFGR1_CONT | ADC_CFGR1_OVRMOD | ADC_CFGR1_DMACFG | ADC_CFGR1_DMAEN );
    #else	/* not ADC_CONT_OVERWR */
    	/* continuous mode, overwrite, right aligned, 12bit,
    	 *	DMA NOT circular -> needs to restart ADC
    	 */
    	ADC1->CFGR1 = ( ADC_CFGR1_CONT | ADC_CFGR1_OVRMOD | ADC_CFGR1_DMAEN );
    #endif	/* ADC_CONT_OVERWR */
    
    	/* clock: synchronous 1/4 PCLK,
    	 *	+ oversampling
    	 */
    	ADC1->CFGR2 = ( ADC_CFGR2_CKMODE_1 |
    					ADC_CFGR2_OVSE | ADC_CFGR2_OVSS_64 );
    
    	/* sampling time */
    	ADC1->SMPR = ADC_SMPR_7_5;
    
    	/* ++++++++++++++++++++++++++++++++++++++++++ */
    	/* channel sequencer */
    	/* enable channel 1 (force), VREFINT, temperature sensor, ... */
    	ADC1->CHSELR = ( 	ADC_CHSELR_CHSEL0 | ADC_CHSELR_CHSEL6 | ADC_CHSELR_CHSEL7 |
    						ADC_CHSELR_CHSEL8 | ADC_CHSELR_CHSEL9 |
    						ADC_CHSELR_CHSEL17 | ADC_CHSELR_CHSEL18 );
    
    	/* ++++++++++++++++++++++++++++++++++++++++++ */
    	/* enable ADC internal voltage regulator */
    	ADC1->CR = ADC_CR_ADVREGEN;
    
    	/* delay for ADC internal voltage regulator stabilization */
    	uint32_t u32WaitVregCnt = ((LL_ADC_DELAY_INTERNAL_REGUL_STAB_US * (SystemCoreClock / (100000 * 2))) / 10);
    	while( u32WaitVregCnt != 0 ) u32WaitVregCnt--;
    
    	/* ADC calibration
    	 *	- before ADC enable
    	 *	- before DMA enable
    	 */
    	ADC1->CR |= ADC_CR_ADCAL;
    
    	uint8_t u8AdcError = 0;
    	uint32_t u32TickStart = LL_GetTick();
    
    	while( (ADC1->CR & ADC_CR_ADCAL) != 0 )
    	{
    		/* timeout check */
    		if( (LL_GetTick() - u32TickStart) > ADC_TIMEOUT_CAL_MS )
    		{
    			u8AdcError = 1;
    			break;
    		}
    	}
    
    	if( 0 == u8AdcError )
    	{
    		/* reset EOCAL bit */
    		ADC1->ISR |= ADC_ISR_EOCAL;
    		u8ErrorPwr &= ~ERROR_PWR_ADC;
    	}
    	else
    	{
    		#if DEBUG_ADC
    			uart_printf("#E ADC_Init() CAL, DMA off\n\r");
    		#endif 	/* DEBUG_ADC */
    		u8ErrorPwr |= ERROR_PWR_ADC;
    		return;
    	}
    
    /* +++++++++++++++++++++++++++++++++++++++++++++++++++ */
    /* DMA settings and start */
    
    	DMA1_Channel1->CCR = 0;
    
    	/* DMA channel selection register, set channel 1, request 0 = ADC => clear C1S */
    	DMA1_CSELR->CSELR &= ~DMA_CSELR_C1S;
    
    	/* set DMA channel memory address register */
    	DMA1_Channel1->CMAR = (uint32_t)&u16AdcDmaBuf[0];
    	/* set DMA channel peripheral address register */
    	DMA1_Channel1->CPAR = (uint32_t)&ADC1->DR;
    	/* set DMA channel number of data register */
    	DMA1_Channel1->CNDTR = (uint32_t)ADC_DMA_BUF_SIZE;
    
    	/* set DMA channel configuration register */
    	/*	PL		Priority Level = very high
    	 *	MSIZE	memory size 16 bit
    	 *	PSIZE	peripheral size 16 bit
    	 *	MINC	memory increment mode
    	 *	CIRC	circular
    	 *		NOTE: even if ADC ist not set to CIRC DMA, we can save some settings
    	 *				if DMA is CIRC
    	 *	*IE		interrupt enables
    	 *		TEIE	transfer error
    	 *		TCIE	transfer complete
    	 *		HTIE	half transfer complete
    	 */
    	DMA1_Channel1->CCR = ( 	DMA_CCR_PL |
    							DMA_CCR_MSIZE_0 | DMA_CCR_PSIZE_0 |
    							DMA_CCR_MINC |
    #if ADC_DMA_CIRC
    							DMA_CCR_CIRC |
    #endif	/* ADC_DMA_CIRC */
    							DMA_CCR_TEIE | DMA_CCR_TCIE | DMA_CCR_HTIE );
    
    	/* clear DMA channel 1 interrupt flags */
    	DMA1->IFCR = DMA_IFCR_CGIF1;
    
    	/* reset variables */
    	u8AdcDmaTc	 	= 0;
    	u32AdcDmaErrCnt = 0;
    	u32AdcDmaTcCnt 	= 0;
    
    /* +++++++++++++++++++++++++++++++++++++++++++++++++++ */
    /* start prep & start */
    
    	/* DMA1_Channel1_IRQn interrupt configuration */
    	NVIC_SetPriority(DMA1_Channel1_IRQn, NVIC_IRQ_PRIO_DMA_ADC);
    	NVIC_EnableIRQ(DMA1_Channel1_IRQn);
    
    	/* enable DMA */
    	DMA1_Channel1->CCR |= DMA_CCR_EN;
    
    	/* enable VREFINT & temperature sensor */
    	ADC1_COMMON->CCR |= ( ADC_CCR_TSEN | ADC_CCR_VREFEN );
    	ADC1_COMMON->CCR |= ADC_CCR_LFMEN;
    
    	/* ADC enable */
    	ADC1->CR |= ADC_CR_ADEN;
    
    	/* ADC ready ? */
    	u32TickStart = LL_GetTick();
    	while( (ADC1->ISR & ADC_ISR_ADRDY) != 0 )
    	{
    		/* timeout check */
    		if( (LL_GetTick() - u32TickStart) > ADC_TIMEOUT_RDY_MS )
    		{
    			u8AdcError++;
    			break;
    		}
    	}
    
    	if( u8AdcError != 0 )
    	{
    		#if DEBUG_ADC
    			uart_printf("#E ADC_Init() RDY\n\r");
    		#endif 	/* DEBUG_ADC */
    		u8ErrorPwr |= ERROR_PWR_ADC;
    		return;
    	}
    
    	/* ADC START */
    	ADC1->CR |= ADC_CR_ADSTART;
    }

     

     

    gbmAnswer
    Graduate
    October 28, 2025

    In the code above you are setting ADC DMAEN and DMACFG bits BEFORE calibration. This might be the problem. Do it AFTER calibration is completed.

    LCEAuthor
    Graduate II
    October 28, 2025

    Bingo! Thanks @gbm , that was it.

    Not only DMA controller enable after calibration, but also the DMA enable bit in the ADC register.

     

    Edit: still interesting that the problem only occurred with setting the ADC_CFGR1_DMACFG bit (-> circular) in ADC1->CFGR1. Anyway...