launching the stm32g0 USART Bootloader without hardware reset
Hello guys,
I am working on project to update the STM32G070 over the air. So basically I receive the binary on ESP32 and then forward the binary over UART to the STM32. I have used pattern 11 to enter the USART Bootloader of the STM32. Then sending the 0x7F to get in synchronization with the STM32.
By only controlling the BOOT0 Pin I cannot enter the USART Bootloader. By pulling the NRST Pin and the BOOT0 Pin I can enter the USART Bootloader successfully . So is it possible to enter the USART Bootloader without hardware reset ??