LCD-TFT project with 1024x768 resolution. Which MCU to use?
Hi guys, sorry if I'm posting this in the wrong area.
I'm starting a project that uses a 1024x768 graphics display and I was wondering which STM32F MCU (LQFP 176pin) would be the better to drive the RGB Panel. I would be using external memory but if there is a MCU with internal memory that can display 1024x768 that would be easier and would make the project cheaper as well.
Can you please let me know as soon as possible as at this stage I'm doing the research on what I need before I purchase all the parts.
Thanks guys and hope to hear from you soon.
Peter