Skip to main content
Graduate
February 21, 2024
Solved

LDO for STM32H573AII3Q

  • February 21, 2024
  • 1 reply
  • 1697 views

STM32H573AII3Q is a 169 pin UFBGA SMPS package. Along with SMPS option, does it also have internal LDO for core supply? Can we use internal LDO to supply core voltage for this package?

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello @madhu1 ,

    Only SMPS is supported by this package. And according to the reference manual:

    SofLit_0-1708509182207.png

    So the package has only one PWR config: SMPS or LDO.

    1 reply

    mƎALLEmAnswer
    Technical Moderator
    February 21, 2024

    Hello @madhu1 ,

    Only SMPS is supported by this package. And according to the reference manual:

    SofLit_0-1708509182207.png

    So the package has only one PWR config: SMPS or LDO.

    madhu1Author
    Graduate
    February 21, 2024

    Hello,

    I think it has both option. Even for SMPS power scheme, there is a LDO shown internal to uC. Refer below image: Please let me know if my understanding is correct.

    madhu1_1-1708515188471.png

     

     

     

    Technical Moderator
    February 21, 2024

    Indeed the LDO is there on the die but it is disabled by HW as already said in RM section 10.5.1.