LED Blinks Automatically on Nucleo-H755ZI-Q Instead of Waiting for User Button Press
Hi all! I'm using the Nucleo-H755ZI-Q board and trying to write a simple program where the LED should turn on (and stay on) only when I press the USER button (the blue one on the board). I’ve shared a screenshot of my code below. The code builds and debugs without any errors, but when I run it, the LED just starts blinking on its own... even when I haven’t pressed the button. What’s more interesting is that when I stop the program in the IDE, the LED keeps blinking, and it only stops if I enter debug mode again. I expected the LED to stay off by default and turn on steadily only when the button is pressed. Also, after flashing and starting debug, I only see a "Resume" button instead of "Run"... Not sure if that means something’s wrong or if it’s normal. Any help figuring this out would be great!
my program