Linearity of HRTim Compare
Hello together,
when inspecting the behaviour of the HRTimer regarding the compare output, I found that with Clk multiplier 32, there is a non-linearity in the compare timing (stepwidth) of about +150 ps (330 ps step instead of 180 ps between adjacent compare values). This seems directly to correlate with the depth of the delay line, as I can see this step equally distributed each 32 steps.
Is this known or is there a way to avoid this behaviour and get a more linear behaviour?
My test setup is:
STM32G474, HRTim1
Channel B: 1 MHz pulses, continious
Channel C: single shot, resettable, triggered by Chan B, variable compare value. Set on compare, reset on period.
I checked the delay of the output C regarding to B. Basically I get quite good results with a standard deviation of appr. 30 ps but I wonder of this non-linear step. The step e.g. happens when changing the compare value from 183 to 184 (or 215 to 216).
Br,
Pascal