low power with STM32U5 and LPUART
I'm trying to port code from STM32L4 to STM32U5.
The STM32L4 code was using the LPUART, with a baudrate of 20k, clocked with HSI but in stop2 mode the HSI was stopped, it was able to wakeup and read incoming data. This configuration was using ~10uA.
I'm trying to do the same with STM32U5 but i think the HSI is not stopped during stop2 so it use ~200uA. AFAIK the knowledge base example keep HSI running.
Is it possible to use the same configuration with the STM32U5 ? If yes, is there an example ?
Or the only solution is to use the LPBAM with STM32U5 (like in LPBAM_LPUART_TransmitReceive) ?
Thanks in advance.