LPUART1 wakeup fail in STOP2 mode
Hello,
I'm using LPUART1 (STM32U0) for modbus communication and using STOP2 mode to go sleep until new modbus query has requested.
Strange things happen, on console I can see prints like "Target is not responding, retrying...".
Here is my clock configuration, which I want to reconfirm

And the STOP2 mode logic, here tried to toggle LED after wakeup, but it is observed that sometimes it works and sometimes not. Actually, if I disable function enterLowPowerMode() then everything works fine also no print message on consol (like "Target is not responding, retrying...")
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
void Scheduler::enterLowPowerMode()
{
HAL_UARTEx_EnableStopMode(&hlpuart1);
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
HAL_ResumeTick();
SystemClock_Config();
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
}
Guide me for the current clock configuration or anything missing to take care while going to STOP2 mode.
Thanks,
Nitin