Skip to main content
Explorer
July 15, 2023
Question

LWIP on Nucleo-H755

  • July 15, 2023
  • 2 replies
  • 1126 views

Hello :)

 

i am working with a nucleo-h755zi.

my goal is to create the following:

1. M7 core running with FreeRTOS and LWIP.

2. M4 Core running bare metal.

 

after using the following instructions (https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308#memory-layout ) i was able to achive (1).

unfortenoutly it seems that while the M7 runs fine and i am able to ping it, the M4 Systick is not OK (uwTick is always 0), i also noticed that this problem is fixed when i disable M7 MPU defenitions.

i suspect that the LWIP stack is somehow blocking or corrupting M4 Data. 

Please advise on how to resolve this, perhaps i am missing something? 

 

thanks for your help and responses in advance :)

    This topic has been closed for replies.

    2 replies

    Visitor II
    November 13, 2024

    Hi. I also have the same board and I've been trying to use LWIP with freeRTOS. I can ping my board with LWIP, but the moment I add freeRTOS, I've been struggling. I get it to ping for almost a minute until it goes to Destination Host Unreachable. Have you been able to get it to ping non-stop? I appreciate any advice.

    Visitor II
    July 16, 2025

    Also stuck on the same problem, any progress to share? Trying to use RMII on the NUCLEO-H755ZI and using the lwIP to get a simple ping but no success