Skip to main content
Visitor II
October 20, 2025
Question

manipulating internet connection speed on ISM43362_M3G_L44 (using b-l475e-iot01a)

  • October 20, 2025
  • 3 replies
  • 176 views

Hi guys, im making system wchis is sampling data from 2 microphone channels.
I need to make it pass at least 8 kHz/8 bit/2ch data which i already did. The problem is that i'd like to increase the audio quality of transmitted data, and it's easy on the DFSDM and microphone site BUT:
The maximum internet speed that i archieved is: 182,4 kb/s and i know from datasheet that it can be up to 72,2 Mb/s ("IEEE 802.11n D7.0 -OFDM-72.2 Mbps -single stream w/20 MHz, Short GI").
So lets get to my code:
I'm using configuration files included in STM example:

  • es_wifi_io.c (there is config of SPI3 (it is working with 10MHz speed and supports up to 20MHz - which must be set if we want to use the max speed of the internet);
  • es_wifi.c
  • wifi.c

These files limit the pocket size of IP frame to 1200 bytes and dont support the fragmentation if we send for example 2400 bytes array.
To simulate and test the bandwidth i assumed it will be best:

1. to reduce timeout of wifi:

#define WIFI_WRITE_TIMEOUT 100
#define WIFI_READ_TIMEOUT 100

(it was originally 10000).

2. Make dummy data before the while loop:

for (i = 0; i < ES_WIFI_PAYLOAD_SIZE; i++) {
			DummyData[i] = 255;
			}

and send as many pockets to measure the speed:

while (1) {
WIFI_SendDataTo(Socket, (uint8_t*) DummyData, (ES_WIFI_PAYLOAD_SIZE), &sentLen, 10, BcastIP, LOCAL_PORT);
}

What i counted in wireshark is that in 1 second i recive 18 or sometimes 19 pockets with 1200 bytes each it is: 182,4 kb/s. Could you tell me what to do to increase the speed of this connection? 
What i thought was to increase the clock speed of SPI3 in es_wifi_io.c file and so I did it... and guess what it didnt work. 
I will be very thankfull with any help.
Filip :)

    This topic has been closed for replies.

    3 replies

    Super User
    October 20, 2025

    i know from datasheet that it can be up to 72,2 Mb/s ("IEEE 802.11n

    To reach this speed, the wi-fi must have a decent host interface: master DMA or, at least, fast SPI with DMA. 10 MHz is not fast.

     

    Filip0Author
    Visitor II
    October 20, 2025

    Yeah, i know i wouldn't get the full speed of 72,2 Mbps with 10MHz, it is said it can be archieved with 20MHz in datasheet: "IEEE 802.11n D7.0 -OFDM-72.2 Mbps -single stream w/20 MHz, Short G".
    The problem is that the speed im getting is very, very low (182,4 kbps).....

    Super User
    October 21, 2025

    To see what is going on the wi-fi side, you can use a wireless sniffer (wireshark or other). If all is good there (no retransmissions, no broken packets) - the problem is somewhere else.