Hello @Smith_023 ,
Thank you for updating post.
The maximum display resolution depends on display characteristics.
You can see on the below an example of 1024x768 display with 30Hz refresh rate calculation.
Firstly, you need to calculate the LTDC pixel clock: pixel clock = Total Width x Total Height x refresh rate = 23.59MHz.
Then, depending on the DSI color coding, it is possible to evaluate the equivalent pixel clock as follows:
As an example, when using one data lanes at 500 Mbit/s: for 16 bits per pixel coding example maximum equivalent pixel clock is 500Mb/s / 16 bpp = 31.25 MHz
In this case the 1024x768 display with 30Hz refresh rate is supported.
Please see AN4860

Please let me know if my reply answer your request?
Thank you.
Kaouthar