Skip to main content
Visitor II
December 14, 2023
Question

MCU consulting STM32F412RGT7

  • December 14, 2023
  • 2 replies
  • 1262 views

May I ask whether ST has STM32F412RGT7 model and Operating temperature to 105°C.TKS!

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    December 14, 2023

    Hello @Zhong and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    according to the DS11139:

    STTwo32_0-1702545478668.png

    The MCU STM32F412RGT7 doesn't exist but we have the STM32F412RGT6 and STM32F412RGT6TR who support a temperature range between -40 to 85 °C and we have the STM32F412VGT7who support a temperature range between -40 to 105 °C.

    For more details on available MCUs you can take a look on the MCU/MPU selector of the STM32CubeMX.

    Best Regards.

    STTwo-32

    Super User
    December 14, 2023

    You can see the available variants in the website of the base model (here STM32F412RG) under "Sample&Buy" tab.

    Also, if you look at the table in "Product selector" tab of the whole series, there is a "Maximum temperature" column, so you can select according to that (e.g. there is a -7 suffixed STM32F412RE - although real availability at distributors may still be questionable).

    JW