Skip to main content
Explorer
October 1, 2025
Question

MCU Selection High Speed SPI and QSPI

  • October 1, 2025
  • 1 reply
  • 194 views

Hello Team,

We are Looking to select MCU Which has High Speed SPI and QSPI in a Single Device ,

High Speed SPI - 50 Mbps to 90 Mbps ( One channel ) to interface External Ethernet Controller 

QSPI  - ( One channel ) -  to interface with External Motion Unit

Both above interface work Independently and simultaeneously. 

Device from MCU Series U5 and H5 Would be preeferable. 

However , Our application is not batttery powered , so no power saving Headache.

 

    This topic has been closed for replies.

    1 reply

    bsutharAuthor
    Explorer
    October 2, 2025

    Hello Andrew,

    Thanks for Update.

    From the Tools , I found Two series which matches considering M-33 Secure core. I..e STM32H5 and STM32U5.

    Since , application is for industrial Automation side , Not Battery Power , So STM32H5 would be fine.

    Same time, I do not Higher Speed. Of Course , Cost is matter.    

    Also, not sure , Whose cummunity Support is better ?

    What is your suggestion on this ?