Skip to main content
Visitor II
October 27, 2023
Question

MDF and ADF: input data from RAM

  • October 27, 2023
  • 2 replies
  • 1631 views

Is it possible to use the awesome MDF and/or ADF on STM32U5 with input data from RAM? I have not found any configuration for BSMX for this. One use case is an high performance external delta-sigma-demodulator (ADC) on SPI with proprietary data format (24 Bit per channel, MSB first, CRC etc.) for providing the sound data. Another use case is an LSM6DSV16XTR, also connected via SPI.

    This topic has been closed for replies.

    2 replies

    ST Employee
    October 30, 2023

    Hello @FB1,

    Input data are only computed by the hardware filter (MDF). The memory transfer is done by the GPDMA.  ADF and MDF have DMA capabilities to unload the software for the data transfer read from the peripheral and written to the memory. Channels 0 to 11 allocated for AHB/APB peripheral to SRAM transfers (in both ways) unless a 2D addressing is required for the memory, or unless the AHB peripheral supports a burst request

    I suggest you to read the AN5593 (specially chapter 3.4.7).

    Best Regards,

    Pierre

    Visitor II
    April 3, 2025

    I would also like to know.  The DFSDM in earlier processors could take data from "RAM" or more importantly from a DMA transfer from some 16 bit device on the SPI bus.  Very useful...

    But the MDF description seems to be lacking this essential feature making the filter useless for my purposes.

    Please, if there is a way to do this, tell us about it.

     

    FB1Author
    Visitor II
    October 31, 2023

    Hello Pierre,

    My question is how to provide input data from RAM for MDF and/or ADF? The DFSDM block at STM32F7 for instance has 'parallel input data registers'. What are the corresponding registers at MDF and ADF or what is a proper configuration for BSMX?