memcpy causes NMI fault in H563
I’m currently debugging an H563 NMI issue. When I execute
memcpy((uint8_t*)record, (uint8_t*)latest_record_addr, 128), the program jumps to the NMI_Handler().
I have already confirmed using the debugger that record = 0x20002608 and latest_record_addr = 0x81ED000, and both are valid addresses. After execution, I observed that the first 16 bytes were correctly copied to the corresponding address, but for unknown reasons, the program jumps to NMI_Handler().
I set a breakpoint in the assembly code of memcpy() and found that the program jumps to NMI_Handler() after executing the cmp r1, r2 instruction. I also confirmed that r1 = 0x81ED011 and r2 = 0x81ED080, both of which are valid addresses.


After executing cmp r1, r2, the program counter will point to 0xFFFFFFA8, and then jump to NMI_Handler().


The first 16 bytes of memory were successfully written.
Has anyone encountered this issue with the H563? Any clues or solutions?
I would greatly appreciate it!