Skip to main content
Graduate
March 1, 2024
Question

Memory

  • March 1, 2024
  • 1 reply
  • 874 views

Can any one confirm that STM32G030k8 MCUs can be implemented for DALI-2 lighting.Is the memory works.

    This topic has been closed for replies.

    1 reply

    Super User
    March 1, 2024

    Which memory? Any STM32 MCU can drive the DALI bus, or anything like it, with appropriate electronics. A device role is also possible. the spec provides plenty of power and very lazy timing.

    Visitor II
    March 2, 2024

    Why is the memory related to external components needed?

    Assuming, for DALI-2 lighting you need anyway an external chip, interface, extension board - why are you asking "if a memory would work"? I assume, the DALI-2 as interface and protocol itself is not supported on MCU: you need external logic.

    A memory should always work (it is internal, if it would fail - your program would crash). Would be your more important question: "how to connect a DALI-2 controller on an MCU?"