Skip to main content
Visitor II
June 7, 2024
Question

Memory Interfacing with STM32H753ZIT6

  • June 7, 2024
  • 1 reply
  • 667 views

Hello Team,

I  need to connect an external NAND flash with STM32H753ZIT6 controller. 

What is the maximum capacity of NAND flash that can be interfaced with the FMC controller on the STM32H753ZIT6?

 

Thanks in advance

    This topic has been closed for replies.

    1 reply

    Graduate II
    June 7, 2024

    Didn't you already ask this?

    NAND access as a block device thru a very small window. Basically as large as you want and can afford. Figure many 100s of GB.

    Consider using eMMC devices