Minimum Clock Speed, and enabling PSSI problem
Hello, I'm just evaluating the STM32H7R3Z8 for a new project. I'm having two issues, possibly with the STM32CubeMX, or maybe I'm just not understanding the part.
1) No matter what I do, I cannot seem to enable PSSI. The combobox is grayed out with "Disable" selected. If I mouse over, it says, "DCMI and PSSI are an exclusive choice". DCMIPP is currently disabled for both Application and Boot profiles, and the combobox if I select DCMIPP is set to "Disable". See:

My reading of the datasheet (p.21) shows the STM32H7R3Z8J6 should have a 16-bit wide PSSI available.
2) I cannot seem to create a power profile running at lower than 300MHz (nor is there any data in the datasheet for power consumption at lower frequencies). Is it possible to run this component at 60MHz? Should I expect similar power consumption to an STM32H5 part at that speed? (Since consumption at 300MHz on the STM32H7 seems roughly equal to 250MHz on the STM32H5)
Thanks!