Minimum Frequency for Bypass mode
Hello Community,
I am working on a use case where I have 4 remote MCUs that ideally should be synced with a host MCU. I however have no way to even install an external precision Clock source on these remote MCU's (due to various environmental & budget limitations), while I can accept a precision reference clock signal from any external device that is off-board ie of PCB via one available differential channel on my CAT6e cables. I wish to seek your insights to confirm my assumptions & clear my doubts if I can use this external Clock source to clock the HSE & replace the lower +-5% stability internal 16Mhz HSI on STM32G0B0 MCUs.
Point #1:
The Datasheet does NOT mention any minimum frequency for the external clock signal to HSE as input clock refernce, so in theory (for sake to my understanding) does this mean I can use a signal as low as 32Khz for driving the MCU? Or am I missing something obvious here?
The Datasheet mentions no minimu frequency limit for an external clock source
Then in theory, can I also use a stable 50/60Hz signal that is available to clock the MCU?
Point #2:
Further I am confused, as the Datsheet of the STM32G0B0RET6 mentions the HSI16 has +-5% stability on the first page, while the internal page on clock charectiristics mentions it has ~1.25% stability
Clock characteristics mentioned inside the Datasheet
Clock stability mentioned on the front page of the same Datasheet!
I am confused, is this a major typo in the datasheet or am I missing something here?
Your insights shall be appreciated.