Missing section IRTIM in STM32U0 RM and more.
1. According to datasheet, STM32U0 family have an IRTIM (Infrared interface). But this section is missing in RM0503. Also in SYSCFG_CFGR1 there is missing IR_MOD and IR_POL bits.
2. In RTC section Figure 297 it is missing RTC_OUT2 and RTC_REFIN pins. See same block for STM32G0 family.
3. In RM0503 section NVIC table 54, I think that PVD_PVM should be PVD / PVM. Also ADC_COMP should be ADC / COMP. WWDG should be WWDG / IWDG. TIM6_DAC / LPTIM1 should be TIM6 / DAC / LPTIM1.
4. Usually each section name ends with an abbreviated name in parenthesis. Ex: Low-power universal asynchronous receiver transmitter (LPUART). And this abbreviated name is also in bookmarks on the left size of each RM. But (LPUART) is not in bookmarks in several RM possible all from the beginning.